cancel
Showing results for 
Search instead for 
Did you mean: 

No wlan0 on DK1 I just received.

BillR
Associate III

I have a pair of DK1 boards I just received that I wanted to get working with wifi direct, but neither even can show a wlan0 interface. In the past I have used a DK2 with buildroot and got the wlan0, and a coworker used stock yocto build on the DK2 and said wlan0 was there too. Is there some problem with the DK1?

#first check:

root@stm32mp1:~# ifconfig -a

eth0     Link encap:Ethernet HWaddr 00:80:E1:42:70:CC  

         UP BROADCAST MULTICAST MTU:1500 Metric:1

         RX packets:0 errors:0 dropped:0 overruns:0 frame:0

         TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

         collisions:0 txqueuelen:1000 

         RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

         Interrupt:57 Base address:0x4000 

lo       Link encap:Local Loopback  

         inet addr:127.0.0.1 Mask:255.0.0.0

         inet6 addr: ::1/128 Scope:Host

         UP LOOPBACK RUNNING MTU:65536 Metric:1

         RX packets:264 errors:0 dropped:0 overruns:0 frame:0

         TX packets:264 errors:0 dropped:0 overruns:0 carrier:0

         collisions:0 txqueuelen:1000 

         RX bytes:16800 (16.4 KiB) TX bytes:16800 (16.4 KiB)

usb0     Link encap:Ethernet HWaddr 66:38:9F:BB:BF:73  

         inet addr:192.168.7.2 Bcast:192.168.7.255 Mask:255.255.255.0

         UP BROADCAST MULTICAST MTU:1500 Metric:1

         RX packets:0 errors:0 dropped:0 overruns:0 frame:0

         TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

         collisions:0 txqueuelen:1000 

         RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

#try load module:

root@stm32mp1:~# modprobe brcmfmac

cfg80211: Loading compiled-in X.509 certificates for regulatory database

cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'

root@stm32mp1:~# lsmod

Module                 Size Used by

brcmfmac             192512 0

brcmutil              16384 1 brcmfmac

cfg80211             503808 1 brcmfmac

galcore              331776 2

stm32_cec             16384 0

cec                   40960 1 stm32_cec

sch_fq_codel          20480 3

goodix                20480 0

ipv6                 417792 30

# still nothing:

root@stm32mp1:~# ifconfig -a

eth0     Link encap:Ethernet HWaddr 00:80:E1:42:70:CC  

         UP BROADCAST MULTICAST MTU:1500 Metric:1

         RX packets:0 errors:0 dropped:0 overruns:0 frame:0

         TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

         collisions:0 txqueuelen:1000 

         RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

         Interrupt:57 Base address:0x4000 

lo       Link encap:Local Loopback  

         inet addr:127.0.0.1 Mask:255.0.0.0

         inet6 addr: ::1/128 Scope:Host

         UP LOOPBACK RUNNING MTU:65536 Metric:1

         RX packets:264 errors:0 dropped:0 overruns:0 frame:0

         TX packets:264 errors:0 dropped:0 overruns:0 carrier:0

         collisions:0 txqueuelen:1000 

         RX bytes:16800 (16.4 KiB) TX bytes:16800 (16.4 KiB)

usb0     Link encap:Ethernet HWaddr 66:38:9F:BB:BF:73  

         inet addr:192.168.7.2 Bcast:192.168.7.255 Mask:255.255.255.0

         UP BROADCAST MULTICAST MTU:1500 Metric:1

         RX packets:0 errors:0 dropped:0 overruns:0 frame:0

         TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

         collisions:0 txqueuelen:1000 

         RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

#For the heck of it:

root@stm32mp1:~# wpa_supplicant -B -Dnl80211 -iwlan0 -c /etc/wpa_supplicant.conf

Successfully initialized wpa_supplicant

Could not read interface wlan0 flags: No such device

nl80211: Driver does not support authentication/association or connect commands

nl80211: deinit ifname=wlan0 disabled_11b_rates=0

Could not read interface wlan0 flags: No such device

wlan0: Failed to initialize driver interface

This is the shipped SD version with 4.19 kernel. I also tried my own Dunfell build with kernel 5.4, same problem with no wlan0.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
BillR
Associate III

Looking through some other comments I noticed it mentioned there is no wifi chipset on the DK1. This might explain it!

View solution in original post

1 REPLY 1
BillR
Associate III

Looking through some other comments I noticed it mentioned there is no wifi chipset on the DK1. This might explain it!