STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I built my image with my STM32MP157F-DK2 board How can I Create a file with this argument check GPU readme file exist.

When I open it with this command,less README-CHECK-GPUCheck GPU =========   GPU can be deactivated by fuse or not present in some SOC   So in case the GPU is not present, you must configure weston on pix-man by creating this file : /etc/default/westo...

Gencay by Associate III
  • 2606 Views
  • 3 replies
  • 0 kudos

modify a CAN sample point

I using a STM32MP-157F-EV1 eval board with linux Version 4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15.CAN receive 500kBit/s fails, if I modify the sample point via an console command it works well. All other Bitrates 125kBit / 250kBit 1MBit a...

MaHa by Associate II
  • 3624 Views
  • 5 replies
  • 1 kudos

Resolved! STM32MP1) Occasionally eMMC boot fail with "CMD13 failed after 5 retries"

​Hi all ~​I have STM32MP157C custom board. My custom board boot over eMMC. Occasionally, my board can not boot over eMMC with error message like below.Can I get some advice regarding this problem?Hardware of eMMC part is the same as EV1 board. ​Thank...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.