STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I created DTS files for my custom board, my DDR configuration is same as stm32mp157A-ev1 board and I am using same mpu. Why some of the CUBEMX generated TF-A DDR registers and Eval registers are different?

EVAL BOARD (stm32mp15-ddr.dtsi)   #define DDR_PCFGR_0 0x00010000 #define DDR_PCFGR_1 0x00010001   My Board (TF-A/stm32mp15-mx-dtsi)   #define DDR_PCFGR_0 0x00000000 #define DDR_PCFGR_1 0x00000000Why are these registers different even though I have th...

Gencay by Associate III
  • 1351 Views
  • 1 replies
  • 0 kudos

Enabling sdmmc3, What will happen?

For my custom board, I will be using emmc on the sdmmc2 and wireless on sdmmc3 so according to this article I have to change linux kernel boot command. Since I am not going to have anything on the sdmmc1 (SD Card) isn't it suppose to boot from emmc w...

Gencay by Associate III
  • 1207 Views
  • 0 replies
  • 1 kudos

Debug SPL with OpenOCD

I would like to bring up the openocd and gdb debugger on a custom board with STM32MP157D processor with 1 GB (2x512MB 16 bit DDR3 chips) x 32 bit. The modified device-tree and SPL gives me the following issue:U-Boot SPL 2022.01-rc3 (Sep 07 2022 - 16:...

Resolved! I built my image with my STM32MP157F-DK2 board How can I Create a file with this argument check GPU readme file exist.

When I open it with this command,less README-CHECK-GPUCheck GPU =========   GPU can be deactivated by fuse or not present in some SOC   So in case the GPU is not present, you must configure weston on pix-man by creating this file : /etc/default/westo...

Gencay by Associate III
  • 2526 Views
  • 3 replies
  • 0 kudos