STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! What data types are used for the fields in the STM header of binary files when the signature/sha256 is generated?

We are trying to verify the signature generated by the STM signing tool. From this link, in the table for "On STM32MP15x lines", we need to know what data type is used for each field when the signature hash (sha256) is created so we can replicate it.

GWu.4 by Associate
  • 1956 Views
  • 1 replies
  • 0 kudos

TF-A v2.6-r1 kernel hang issue?

I have a custom build on the stm32mp157f dk2.stm TF-A v2.6-r1 or vanilla TF-A v2.7, using sp_min.stm U-boot 2020.10-r2 or vanilla Barebox-2022.06.I've also tried U-boot 2021.10-r1, but that one crashes the kernel even earlier.Kernel: vanilla 5.18/van...

Hi: I can't find qmake in 4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15. When I use qtcreater5.15, I can't create STM32 code.

When I use cmake,/opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sysroots/x86_64-ostl_sdk-linux/usr/share/cmake-3.22/Modules/CMakeTestCXXCompiler.cmake:62: error: The C++ compiler "/opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-k...

zxiao.4 by Associate III
  • 1537 Views
  • 1 replies
  • 0 kudos