STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Issue booting with eMMC on STM32MP157F-Eval board

Hello STM-Team,I am working with STM32MP157F-Eval board. The SD card and NAND booting are working fine. But, getting issues while booting with eMMC.I have tried a workaround which seems to be working and I want to make sure if it is the right way of ...

Playing Video with gst-launch

Hi,I want to play a video from mounted USB stick. Once USB plugged the host, I mount it with "mount /dev/sda1 /mnt" and than quit the psplash screen with "psplash-drm-quit" on target. After that, trying to play a video with "gst-launch-1.0 playbin ur...

stm32mp1 spi transaction slow down main application

Hi AllI have disabled the second core to validate one of old product, which runs on single core,and same application cpu usage i have seen is 90-95 %and same application runs and does the same spi transaction, i am seeing the cpu usage is 57%all cons...

Ara.1 by Senior
  • 1050 Views
  • 5 replies
  • 0 kudos

Resolved! How to do SRAM3 shared memory mapping in user space for data transfer between the A7 cores and the M4 core.

I want to use part of the SRAM3 shared memory for data transfer between the A7 cores and the M4 core. On the A7 core I used mmap on /dev/mem to remap the sram to user space and copy the data to/from the SRAM3 buffers. The result is however not stable...

Kvan .6 by Associate II
  • 1195 Views
  • 4 replies
  • 0 kudos

Resolved! Add support of MLC NAND in STM32MP157C Board

Hello STM-Team,We are developing a custom board based on STM32MP157C-Eval board.In that, we are planning to have MLC NAND Part number #MT29F16G08CBACAWP:C instead of SLC NAND.For Software point of view, I want to understand that if the existing NAND ...

Use Openvino and / or ONNX in STM32MP1

Is it possible to use AI frameworks like ONNX and / or Openvino (and related accelerators like movidius, GPU) on STM32MP1? I took a look but I found only examples with tensorflow lite and Coral devices (i.e. https://github.com/STMicroelectronics/meta...

EBelt.1 by Associate II
  • 531 Views
  • 1 replies
  • 0 kudos

Resolved! How to release port 8888.?

I have a problem. My application should use port 8888. I wrote an application in Python 3.5 that uses the address and port 8888 that I need. But Linux issues a diagnosis that port 8888 is already occupied by another task. How to release port 8888.? T...

Vlaty.1 by Senior
  • 1925 Views
  • 10 replies
  • 0 kudos