User Activity

Hi STM-Team,We are facing problem while using multiple USART in parallel on STM32MP153C running Linux kernel v5.4.Our application contains two separate threads communicating on two separate RS485 ports in parallel at every ~10ms. After further debugg...
Hi STM-Team,We are trying to enable/configure HS200/HS400 mode in eMMC on STM32MP157F-EV1 evaluation board.We are using the stm32mp157f-ev1.dts device tree and we have configured the eMMC node as shown in below screenshot. As per the documentation, w...
Hi STM-Team,We have the custom board based on the STM32MP157C-Eval board.In that, we are not able to access the eMMC from u-boot command prompt. Currently, we are booting from SD card and able to access it from u-boot command prompt.We are able to se...
Hi STM-Team,I am working with STM32MP1 evolution board. It has 512MB of RAM memory. I want to load some custom data (1024 byes) in the last some offset of RAM memory (~500MB offset address). So, I am trying to use below command from u-boot prompt. Bu...
Hi STM-Team,I am working with STM32MP157F-Eval board. I have enabled and tested secure-boot flow as per https://wiki.st.com/stm32mpu/wiki/STM32MP15_ROM_code_secure_boot.Now, I am looking for next security part for singing-verification of kernel & DTB...
Kudos from