STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ALSA is interfering the DCMI camera

When using DCMI camera capture and at the same time play or record audio, there is bad interference in the camera picture. I'm using Linux and ALSA libraries in a platform based on STM32MP157C. Maybe some DMA problem ? The audio is using SAI as with ...

Ronte.1 by Associate II
  • 829 Views
  • 0 replies
  • 0 kudos

Resolved! Is VBAT needed for secure boot ?

Hello,In the wiki I have found these lines:5.3 Non-volatile counters↑Each certificate embeds a non-volatile counter value that is checked to control anti-rollback mechanism.There are two non-volatile counters: - Trusted non-volatile counter - Non tru...

How to add OSDP RS485 protocol in STM32MP157 yocto build?? Namely, LibOSDP ( https://libosdp.gotomain.io/libosdp/build-and-install.html )

I have to use OSDP protocol over stm32mp157 by using LibOSDP in my yocto build. How to build it, from where to start?(sorry but i am new to linux thus maybe a silly question, but any guidance would really be appriciable )

SChat.2 by Associate II
  • 1322 Views
  • 1 replies
  • 0 kudos

Resolved! STM32MP15 OTP Mapping Wiki

Hey I found a strange documentation on your wiki pagehttps://wiki.st.com/stm32mpu/wiki/STM32MP15_OTP_mapping 3: 14-7 (8 bits)UART instances disablingIf it is different from zero, then each bit disables an UART instance.Collapse0b00000001: reserved0b0...

BBoge.2 by Associate II
  • 1995 Views
  • 5 replies
  • 0 kudos