User Activity

I'm getting these errors on the consoles when FSBL (TF-A) is trying to download SSBL (U-Boot). What could this DFU error be? I've added the following to the U-Boot DTSI file so it ignore USB OTG VBUS and USB OTG ID. I've tried this using Linux and Wi...
I've been validating my DDR interface with DDRUTIL through the CubeMX DDR Interactive which seems to pass the tests. When I boot TF-A it is failing both address bus testing for 1's and 0's. But I can run this same test through DDRUTIL and it passes. ...
I'm having trouble getting TF-A to start from USB DFU using the STM32Programmer CLI. Here's what I get:$ ./xpro_uboot_prgm.sh ------------------------------------------------------------------- STM32CubeProgrammer v2.11....
I'm using STM32CubeProgrammer to flash my custom target using an STM32MP153AAA MPU. I have onboard a 4GB eMMC memory. During the programming process through DFU all seems good and finishes at 100% but then sits for a bit and I get errors. Seemingly T...
Building per the Developer Package Device Tree Building WikiUsing STM32MP1-Ecosystem_v4.0.0Verified libssl-dev and libncurses have been installedopenssl version 3.0.0 is presentconfirmed libcrypto.so is present at usr/lib/x86_64_linux-gnu[fiptool] Cr...