STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP1 + STPMIC1A PMIC Power issue

Hi ~I am using STM32MP157C MPU + STPMIC1A for my custom board with ecosystem 4.1And unfortunately I'm wrestling with some problem regarding PMIC.I produced 30 boards for sample.Some board is working fine but some board has power issue.1) Custom board...

1.jpg 2.jpg 3.jpg 4.jpg

We have developed a custom board using STM32MP157AD3 chipset and STPMIC. We did develop a dts using CubeMX and did all the patches as mentioned in Lab documentation. But we came accross 2 errors.

When we use the PMIC values from DK2 example.1 . ERROR:  regul ldo3: max value 750 is invalidWARNING: register_pmic:600 failed to register ldo3PANIC at PC : 0x2fff05cb2 Next we tried setting the ldo3 max, min values to 3V and 1.8V and it was working ...

NP by Associate II
  • 12730 Views
  • 11 replies
  • 0 kudos

Resolved! STM32MP15 ECO 5.0.0. Documentation does not provide a information how to create a new FIP

As in a different post, The TF-A build did not create the FIP binaries after deleting the FIP build folder.This article does not describe how to create a new FIP binary. only how to update. very confusing !The fiptool does provide a create function b...