cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP15 OTP Mapping Wiki

BBoge.2
Associate II

Hey I found a strange documentation on your wiki page

https://wiki.st.com/stm32mpu/wiki/STM32MP15_OTP_mapping

3:

14-7 (8 bits)UART instances disablingIf it is different from zero, then each bit disables an UART instance.

Collapse

  • 0b00000001: reserved
  • 0b00000010: disable USART2
  • 0b00000100: disable USART3
  • 0b00001000: disable UART4
  • 0b00010000: disable UART5
  • 0b00100000: disable UART6
  • 0b01000000: disable UART7
  • 0b10000000: disable USART8
  • 0b11111111: all UART instances are enabled.

Why is all enabled when all UARTS are 1?

I set everything to 1 but I get messages on the serial console.

Do you have a hint for me?

Greetings

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
OlivierK
ST Employee

Hi BBoge.2 (Community Member)

0b11111111: all UART instances are enabled

This is a protection to avoid bricking all the USART ports by mistake.

If you want to disable all UART instances at once, you should use OTP3.23-16 boot source disable instead (disable UART boot source).

Rgds,

Olivier


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
BBoge.2
Associate II

If I set all bit to 1 in the otp 3. The serial communication will work as before.

For example:

fuse prog -y 0 3 0x185B7F04

But after stm32key close the serial communication is still open.

OlivierK
ST Employee

Hi BBoge.2 (Community Member)

0b11111111: all UART instances are enabled

This is a protection to avoid bricking all the USART ports by mistake.

If you want to disable all UART instances at once, you should use OTP3.23-16 boot source disable instead (disable UART boot source).

Rgds,

Olivier


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
BBoge.2
Associate II

Hey Oliver,

and when I try to disable the serial console that prints everything over UART?

Greetings

Benedikt

PatrickF
ST Employee

Hi @BBoge.2​ 

This OTP is related to BootROM UART usage (i.e. connection with CubeProgrammer).

This has nothing to do with Console usage.

I'm not expert, but I think console should likely be disabled using Device Tree.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
BBoge.2
Associate II

Hi Patrick,

okay maybe there was a miss understanding from point of view.

Thanks for your support.

Greetings

Benedikt