2023-01-09 1:17 PM
Building per the Developer Package Device Tree Building Wiki
Using STM32MP1-Ecosystem_v4.0.0
Verified libssl-dev and libncurses have been installed
openssl version 3.0.0 is present
confirmed libcrypto.so is present at usr/lib/x86_64_linux-gnu
[fiptool] Create fip-stm32mp153a-xpro-mp1-mx-optee.bin fip binary into 'FIP_DEPLOYDIR_FIP' folder...
fiptool: error while loading shared libraries: libcrypto.so.1.1: cannot open shared object file: No such file or directory
[fiptool] Done
Solved! Go to Solution.
2023-01-12 9:05 AM
Hi Jim,
When checking the build commands you are using, you are following the chapter §5.2 in README.HOW_TO.txt, and I recommend you to not launch "make stm32mp15_defconfig" first, only the second make command with all the given parameters.
So you can try
One more point, in order to take into account your dt file generated from CubeMx, you will have to update arch/arm/dts/Makefile, in order to add it on the CONFIG_STM32MP15x. Do not know if already taken into account on your side?
Thank you
Jean-Philippe
2023-01-10 2:07 AM
Dear @Community member
This issue must be corrected with new STM32MP1-Ecosystem_v4.1.0.
However, you can probably cherry-pick some commits on https://github.com/STMicroelectronics/meta-st-stm32mp:
Thank you
BR
Jean-Philippe
2023-01-10 6:58 AM
Thanks Jean-Phillipe, I'll give that a go and see what happens.
2023-01-10 3:34 PM
Jean-Phillipe,
I installed 4.1.0 today and all looked good. Just tried to build with my device trees and the libcrypto error did go away which is awesome however there seem to be a few more errors at the u-boot stage which aren't very clear keeping the build from completing. I'm not doing anything special, simple CubeMX device trees based on my target hardware. Is anyone actually building successfully with this stuff?
Using /home/jkellar-pulse/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2021.10-stm32mp-r2-r0/u-boot-stm32mp-v2021.10-stm32mp-r2 as source for U-Boot
/home/jkellar-pulse/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2021.10-stm32mp-r2-r0/u-boot-stm32mp-v2021.10-stm32mp-r2 is not clean, please run 'make mrproper'
in the '/home/jkellar-pulse/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2021.10-stm32mp-r2-r0/u-boot-stm32mp-v2021.10-stm32mp-r2' directory.
make[2]: *** [/home/jkellar-pulse/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2021.10-stm32mp-r2-r0/u-boot-stm32mp-v2021.10-stm32mp-r2/Makefile:1858: prepare3] Error 1
make[2]: Leaving directory '/home/jkellar-pulse/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2021.10-stm32mp-r2-r0/build/stm32mp15_defconfig'
make[1]: *** [Makefile:177: sub-make] Error 2
make[1]: Leaving directory '/home/jkellar-pulse/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2021.10-stm32mp-r2-r0/u-boot-stm32mp-v2021.10-stm32mp-r2'
make: *** [/home/jkellar-pulse/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2021.10-stm32mp-r2-r0/u-boot-stm32mp-v2021.10-stm32mp-r2/../Makefile.sdk:142: uboot-stm32mp15_defconfig] Error 1
~/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23 ~/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/sources/arm-ostl-linux-gnueabi
~/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/sources/arm-ostl-linux-gnueabi
2023-01-11 7:19 AM
Hello @Community member
Just make a try on my side, and no issue seen.: STM32MP157F-DK2 board selected.
Could you please tell me more about different below steps?
Thank you
Jean-Philippe
2023-01-11 8:08 AM
Hello JeanPhilippe
I can build the EV and DK boards sets. For my custom target I'm not specifying a board. I've generated DTS files from an IOC in CubeMX. Its for an STM32MP153A. Attached is my project information (e.g. the IOC, DTS files, etc.)
To answer your questions:
No board selected. Custom target spec'd in CubeMX for STM32MP153A. DTS files generated by CubeMX.
DTS file names - stm32mp153a-xpro-mp1-mx.dts
I assume this is in reference to getting the sources, in particular U-Boot. Used the TAR file from the SOURCES download. Followed the README.HOW_TO.txt file in each source (i.e. kernel, tf-a, op-tee and u-boot) to setup and do an initial build of everything.
I've written a script to perform all command line sets from the README files. Script is attached. Specifically for U-Boot the command line is:
make stm32mp15_defconfig
make -f $PWD/../Makefile.sdk UBOOT_CONFIG=trusted UBOOT_DEFCONFIG=stm32mp15_defconfig UBOOT_BINARY=u-boot.dtb FIP_CONFIG="optee" DEVICETREE=$DTS_NAME all Thanks,
Jim
2023-01-12 9:05 AM
Hi Jim,
When checking the build commands you are using, you are following the chapter §5.2 in README.HOW_TO.txt, and I recommend you to not launch "make stm32mp15_defconfig" first, only the second make command with all the given parameters.
So you can try
One more point, in order to take into account your dt file generated from CubeMx, you will have to update arch/arm/dts/Makefile, in order to add it on the CONFIG_STM32MP15x. Do not know if already taken into account on your side?
Thank you
Jean-Philippe
2023-01-12 9:55 AM
Hi Jean-Philippe,
Yes! Very good. Seems that I'm now building a complete set of binaries. The solution is in two parts though one of which doesn't seem documented that I could find, therefore I hadn't done it.
After that all was good.
Thanks,
Jim
2023-01-13 12:12 AM
Hi Jim,
Good to hear this is ok now on your side!
Thank you for your feedback.
I will check how to improve guidelines in the README.HOW_TO.txt.
Thank you
BR
Jean-Philippe
2023-01-13 1:52 AM
Hi Jim,
I would like to complete my answer for your point2.
When checking the full build mecanism, DEVICE_TREE_EXT build variable exist to cover your need (using DT files from CubeMx). it avoid making patch in DTS Makefile.
You can use it as below example with <newCubeMxDT>
$ make -f $PWD/../Makefile.sdk UBOOT_CONFIG=trusted UBOOT_DEFCONFIG=stm32mp15_defconfig UBOOT_BINARY=u-boot.dtb DEVICETREE=<newCubeMxDT> DEVICE_TREE_EXT=<newCubeMxDT>.dtb all
We will check to highlight this way of working (wiki page or README.HOW_TO).
Best regards
JJean-Philippe