STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

QEMU on stm32mp157

I want to emulate the stm32mp157 on qemu. I have been taking the kernel image and initrd from yocto build, but it is not loading the kernel. using the following commandqemu-system-arm \-M virt -smp 8,sockets=1,cores=4,threads=2 -m 4G \-cpu cortex-a7 ...

Resolved! STM32MP157FAD1

Hello,I would like to ask you few questions since I have some unclearances about STM32MP157F MPU:1. If 933MHz DDR3L RAM was connected to the MPU according to the schematic, will the MPU automatically underclock it to max 533MHz?2. Is it possible to c...

filip1785 by Associate II
  • 1770 Views
  • 1 replies
  • 1 kudos