cancel
Showing results for 
Search instead for 
Did you mean: 

QEMU on stm32mp157

junaidh12
Associate

I want to emulate the stm32mp157 on qemu. I have been taking the kernel image and initrd from yocto build, but it is not loading the kernel. using the following command

qemu-system-arm \
-M virt -smp 8,sockets=1,cores=4,threads=2 -m 4G \
-cpu cortex-a7 \
-device virtio-tablet-pci \
-device virtio-keyboard-pci \
-device virtio-net-pci,netdev=net0,mac=52:54:00:12:34:02 \
-device virtio-gpu-pci \
-device virtio-rng-pci,rng=rng0 \
-netdev tap,id=net0,ifname=$TAP,script=no,downscript=no \
-object rng-random,filename=/dev/urandom,id=rng0 \
-serial mon:stdio -serial null -nographic \
-initrd senecos-image-stm32mp1-ems-c2-faa1-20230803140050.rootfs.cpio.gz \
-kernel Image \
-append 'root=/dev/ram0 rw debugshell ip=192.168.7.2::192.168.7.1:255.255.255.0::eth0:off:8.8.8.8 console=ttyAMA0 console=hvc0 '
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
RhSilicon
Lead

I found this reference, I don't know if it helps in your case:

(2021-06-28) STM does not provide direct support for qemu, many STM32MP1 boards exist that makes the use of QEMU not relevant.

However it should be possible by setting the right Yocto machine : https://docs.yoctoproject.org/dev-manual/qemu.html

https://community.st.com/t5/embedded-software-mpus/does-stm-provide-yocto-qemu-support-for-stm32mp1-family/td-p/198838