STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP1 ETH_PHY_INTN

Hello! I am developing a custom board based on STM32MP151C MPU (TFBGA 361pins) with a RMII Ethernet PHY, and I have a simple question regarding to the PHY interrupt signal -sorry if this is a duplicated question, I haven't found a related topic in th...

jmglez by Associate
  • 2539 Views
  • 2 replies
  • 0 kudos

Resolved! Can't run st-example-image-qt QT examples on a custom board based on STM32MP153C with RGB panel

I'm trying to run QT examples on a build created using st-example-image-qt (Ecosystem v2.1) on our custom board. We have a simple RGB display 800x480 resolution, so I modified the cursor.json on the board as follows{ "device": "/dev/dri/card0", "outp...

NBhat.1 by Associate III
  • 4200 Views
  • 5 replies
  • 0 kudos

Resolved! STM32MP157: CAN does not receive anything

Hello,I am using a STM32MP157C development board from Myirtech and trying to interface the board with a CAN device.I am able to bring up the can0 interface. It can send data, I can see it from oscilloscope over Can Hi and Lo pins. The dmesg output is...

mertt by Associate II
  • 3078 Views
  • 3 replies
  • 0 kudos

OPTEE panic fixed_regulator_probe failed

First time trying to get OPTEE working on custom board. The boot stops when OPTEE panics NOTICE: CPU: STM32MP157AAC Rev.Z NOTICE: Model: STMicroelectronics custom STM32CubeMX board - openstlinux-6.1-yocto-mickledore-mp1-v23.06.21 NOTICE: BL2: v2.8...

jhi by Senior
  • 2249 Views
  • 1 replies
  • 0 kudos