STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

hello.We design a board based on ev1,we use silicon image rgb/hdmi bridge ,but it dosen't display on moniter

 sii902x 1-0039: Linked as a consumer to regulator.3[  2.001069] sii902x 1-0039: Linked as a consumer to regulator.4modetest -M stmEncoders:id   crtc  type  possible cstcs possible clones28   31   D@I   0x00000001   0x00000000Connectors:id   encoder ...

Cliqi by Associate
  • 1656 Views
  • 2 replies
  • 0 kudos

Uboot DFU not working

We have build a device that looks like DK2 but we have a NAND memory instead of SD card and we work on an IO supply of 1.8V instead of 3.3V. We can load the fsbl and U-Boot with STM32cubeprogrammer, but U-Boot resets the usb and the STM32cubeprogramm...

JVerb.1 by Associate II
  • 4365 Views
  • 9 replies
  • 1 kudos

Resolved! Copy file into bootfs partition

Using the Distribution Package for STM32MP1 I wrote a simple function to copy some file to the rootfs image and execute fine-tuning commands:my_postprocess_function() { cp -dr /home/osboxes/Documents/overlay/* ${IMAGE_ROOTFS} ln -s /lib/systemd/sys...

Mark81 by Associate III
  • 1640 Views
  • 1 replies
  • 0 kudos

Problems with ecosystem & STM32MP157C-EV1 and how to get STM32CubeProgrammer working with it

I'm trying to get STM32MP157C-EV1 board working with the STM32Cube ecosystem.I've had a lot of issues - the documentation isn't well "connected" re. no "getting started" guide with the board. I eventually found the wiki pages - would be *very* useful...

DEdwa.1 by Associate II
  • 4022 Views
  • 5 replies
  • 0 kudos

DMA and DMAMUX on STM32MP157 DK

Hi, I'm trying to get DMA2 requests working, using TIM and HAL. Iam using TIM5_CH2 and iam not sure which DMA2 stream should be used here (i use stream1). Creating PWM signal isn't a problem, but i want to change duty cycles (very common problem) by ...

KDehm by Associate III
  • 1594 Views
  • 1 replies
  • 0 kudos