STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! OTP Bits Cannnot read

Hi All.I use discovery board of STM32MP157F-DK2 .So I want t to try  read OTP Bits via STM32CubeProgrammer , But I find 2 errs.The err things search ST Community, I fund it. Can't read OTP bits on STM32MP157C-DK2 using STM32CubeProgrammer So I Try to...

Yocto ST-linux headless distribution

Hi there, I'm building an ST-Linux distribution with Yocto (ST Distribution package) on a custom board (based on STM32MP153), and, now that I've tested it, I need to optimize the final image.My distribution should be completely headless (so no HMI an...

SScar.2 by Senior
  • 1389 Views
  • 0 replies
  • 0 kudos

Resolved! run Weston fail on Buildroot

 Hi,The MP157F-DK2 comes with an SD card attached. Weston (ver 5.0.0) with DRM works well.But if I want to run Weston(ver 10.0.1) on Buildroot, it will fail.Do I need to build more packages for Weston?I am using the version of Buildroot.a. buildroot:...

wG.1 by Associate II
  • 3724 Views
  • 1 replies
  • 1 kudos

Seeking Guidance on Using Altium Designer for STM32 PCB using it's design files directly

  *I've imported successfully of STM32mp157 dk-1 board 's schematics in altium designer and I don't know whether this processor is over advanced for application or it is must need to use for our product. even though I'm newbie with lesser yr of exp ,...

mbed_engr by Associate II
  • 5232 Views
  • 0 replies
  • 0 kudos

STM32MP1 & ThreadX RTOS

Hi, during Embedded World I got MP135F devkit. I'm not into Yocto, but guy from ST told me, that MP1 can be used with RTOS but with halved max frequency. I have experiance with ThreadX on H735.Can you hint me how to start? Are there any tutorials? I ...

Pyrograf by Associate II
  • 7295 Views
  • 8 replies
  • 4 kudos