ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CR95HF echo command retuens 0x0E

I am attempting to connect to one of ST's CR95HF NFC chips, but I can't get it to respond correctly to the echo command.1) Reset CR95HF by toggling the IRQ line2) Set chip select line low3) Send two bytes : 0x00 0x55 = Command Echo4) Set chip select ...

Resolved! cr95hf Residual bits in last byte [0x90]

Hi,I am reading mifare desfire tag which is iso14443-4 compliant using cr95hf.Most of the time, communication is completed successfully but sometime, i am getting 0x90 result code when using SendRecv command.0x90 EUnintByte Residual bits in last byte...

ksevil by Associate
  • 1017 Views
  • 1 replies
  • 0 kudos

Resolved! ST25R3911B: Lower the output power

Hello,I am working with an NFC reader with an ST25R3911B chip. The problem I am experiencing is the output power. The power emitted by the antenna is too high; therefore, my task is to reduce the transmitted power.To do this I have relied on reading ...

Resolved! Decrease the totalDuration of RFAL software Library

Hello,I added the RFAL software library to my existing wireless charger project.When I set totalDuration to 50U, there are cases where it cannot detect the card. I get better results when I set totalDuration to 25U. Will it cause problems if I reduce...

silae by Associate
  • 1256 Views
  • 3 replies
  • 1 kudos

Resolved! ST25R3916B RFAL library question

Hi,I have a X-NUCLEO-NFC08A1 and trying to use ST25R3916B RFAL library with nRF5340 from nordic semiconductor. SPI communication and initialization are working. I am running  demoCycle() function from demo_polling.c. However, in the logs, I receive a...

Resolved! RFID Solution required

Hi ST Micro Team. We are planning to start a pilot project on the use of RFID in our office, We want to to place the tags on the laptops so that whenever an engineer with laptop  exits a room the reader should detect. Could you please suggest a possi...