ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Which tag to read/write with NFC03A1

Hi,I have tried to search the forum, but not been able to find a clear answer.I am very new to NFC and have started by acquiring the NFC03A1 (ST25R95) together with a NUCLEO board (F446RE).My hopefully simple questions are:1. Is it possible to write ...

tyassin by Associate III
  • 700 Views
  • 1 replies
  • 0 kudos

Resolved! Industrial NFC reader for ST25DV04KC

Hi,I'm developing firmware for embedded with NFC chip ST25DV04KC (ISO15693 type 5).SDK Discovery based on CR95HF is used for development NFC interface. SDK included DLL for creating applications on PC.Can anyone recommend industrial (device ready for...

Resolved! FTM mailbox message length

Project : STM32L476RG-Nucleo\Applications\X-NUCLEO-NFC04A1\FTM For read, you always add one to the result of the length read:  *msg_len = mblength + 1; Seems reasonable when mblengh is 255 , and you add one to read 256 bytes ,  which is the max mail...

DS.4 by Senior II
  • 820 Views
  • 1 replies
  • 0 kudos

Resolved! X-NUCLEO-NFC08A1 : Change to Single-ended Antenna?

Hello,I have a question about X-NUCLEO-NFC08A1 Evaluation Board.The evaluation board is configured with a differential antenna by default, but I would like to change it to a single-ended antenna.Is there any guidelines I can use when making changes? ...

mhbaek by Associate
  • 745 Views
  • 1 replies
  • 0 kudos

Resolved! st25r3911bdiscocomm.dll?

is some buddy can help me with ST25R3911BDISCOComm.dll I want to present password and write password  what is the appy to use to pressent the password and write and some decumention about the appy   thanks  Eliahu Roash

Resolved! ST25R3918

Can you provide more specific codes for the ST25R3918? I need to program the chip for both card emulator mode, and reader mode.I'm highly interested in knowing the correct registers configuration as well as the NDEF protocol.Best regards,Cairo

Cairo by Associate II
  • 1283 Views
  • 4 replies
  • 0 kudos