Resolved! phone did not read en.x-cube-nfc7
what would you like to know?I have downloaded 'en.x-cube-nfc7' according to the instructions,but the ST25 tap app of my phone did not read the "www.st.com/st25-demo" link. What should I do?
what would you like to know?I have downloaded 'en.x-cube-nfc7' according to the instructions,but the ST25 tap app of my phone did not read the "www.st.com/st25-demo" link. What should I do?
Hi,Im using the Embedded Lib.Im experimenting with the demo_ap2p_prop. I want to send a Hex Array as message instead of a string array. Do i use the same funktion?Is there a diffrent with the size ?or is there a other way to send Hex Data ?err = dem...
Hi Everyone.I have tried test NFC use Nucleo-L152RE and X-Nucleo-NFC06A1.I use STM32duino X-NUCLEO-NFC06A1 example to test. It run normally with SPI interface.But when I change it to I2C interface, it can't run.Hardware modification: • so...
I need a small form factor RF ID Reader (max space available for reader antenna is 60mm x 40 mm) and max tag size is 55mm x 13 mm. Can someone help me to find out the best possible RF ID reader and Tag solution (LF/HF/UHF)? Any design consultant?
Why am I unable to read NDEF information in the STSW-ST25001 APP using the following code, with no messages being displayed?
I am working with an App developer to read/write to an ST25DV Dynamic Tag. The project does the following:1 App writes to the ST25DV a short NDEF Text record (15 bytes), the App then goes into some kind of wait mode2 Host micro reads the tag using I...
Hi there,I am a beginner of using customize board to build a project for reading a ISO 144443-4 card .Due to the environment require a higher power output of the reader, therefore i chose ST25R3917 as my rfid SOC. But during the firmware developing ...
We use dev. kit: ANT7-T-ST25DV64KC with app version: ST25NFCTap version V3.7.0 / ST25SDK: 1.10.0 public version. Q: I try to write binary data from file to it. I succeed in sending 4096 bytes. But when I try to send larger files it fails (tried 8192 ...
Hi,Im using the Embedded Lib. I want one device to be a Target and the other the Initiator in every connection. Im trying to help me with the Ap2p example but couldnt fint anithing that tells me what the devices role is.
I used the I2C example in X-CUBE-NFC7 to write "hello the world" and wanted to read the data from the phone, but according to the above code the phone does not show any NDEF information, what should I do?/* USER CODE BEGIN Header *//** **************...