ST25 NFC/RFID tags and readers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How about STEVAL-SMARTAG1 No power mode?

Currently purchased with the STEVAL-SMARTAG1, it was discovered that the capability collected through the ST25 powers the L0 via EH pin VDD while collecting data from the sensor. I need to collect signals by thermocouple, which is the same transmissi...

Resolved! IOS NFC-TAP doesn't read FTM buffer

Hi everyone, I would like use FTM feature of ST25DV.I develop the code to write EEPROM and buffer of FTM, I can read this buffer with developed Kit and ST25PC-NFC software.But I can't use APP for IOS NFC-TAP because it doesn't read FTM buffer. why?

AGarc.8 by Associate
  • 835 Views
  • 3 replies
  • 0 kudos

Resolved! Problem with ST25R Antenna Matching Tool

 Hello everyone, for my project I am using the X-Nucleo-NFC08A1 board. In addition, I am using an external antenna that I operate differentially. The antenna is connected to the board via an SMA connector. I know that I should also adjust the matchin...

MicrosoftTeams-image.png

Resolved! Access Levels for ST25 Tags

Good morning, currently I'm working on this task is to set the tag to have a different access levels.I downloaded IOS "NFC Tap" App to try out and there's this feature called, "Area Security Status".My question is,for "Readable, write protected by pa...

MaoFeng by Associate II
  • 603 Views
  • 1 replies
  • 0 kudos

Resolved! ST25 NAK after 3 commands

Hello,I have a really weird behaviour for my chip which I can't really figure out. Basically, I am using only the commands from the ST25DV library (st25dv discovery board).After 2 function calls (for example present password and disable RF) the subse...

robertp by Associate II
  • 2579 Views
  • 7 replies
  • 0 kudos

Resolved! STSW-ST25SDK001 ST25DemoApp Example Issue

Good afternoon, currently I want to write a simple NDEF File in the tag's EEPROM by using ST25R3916-DISCO kit.I will attach the guide pdf, "ST25PcDemoApp_software_guide" at below for reference.I faced this problem after I added JARs into "Java Build ...

MaoFeng by Associate II
  • 1762 Views
  • 3 replies
  • 0 kudos