ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How To kill a TAG ?

I try to Kill a TAG, I'm using different configurations but don't obtain a different answer.I believe if a Kill a Tag, It's not more possible for my reader to identify her, but after I using the kill command my Tags still read by my reader.I want to ...

0693W00000BcU7sQAF.png
GPaiv.1 by Associate III
  • 1426 Views
  • 1 replies
  • 0 kudos

Resolved! Alternative MCU to work with ST25RU3993

Hi everyone,I am currently testing the UHF RFID board from ST (ST25RU3993-HPEV) and the eval board is using STM32L476RGT6 (Arm®(a) 32-bit Cortex®-M4) as the MCU. Our testing so far has been good and we would like to design our own RFID reader based o...

TNgo.1 by Associate II
  • 692 Views
  • 1 replies
  • 0 kudos

Resolved! st25r3916 - st25r3918 compatibility

Hello,I wanted some more clarification on the st25r3918 chip, it is very interesting as well as cheap compared to st25r3916 and covers my needs.are they interchangeable? do they have pin to pin compatibility? the firmware has not yet been released or...

Resolved! update firmware using ST25 NFC App V.3.6.0

4 Months ago, we completed the design of a product, where we can update the firmware via ST25DV64K using ST25 NFC App. After installing the new version (NFC TAP App V.3.6.0), it doesn't work anymore. Can we get access to the previous version of the a...

JNeig.1 by Associate II
  • 1159 Views
  • 3 replies
  • 0 kudos

Resolved! About the value of MB_MODE of ST25DV64K at power-on

Hello allI use ST25DV64K.I am always set the MB_MODE of ST25DV64K to 1 after power-onAfter setting the value to 1, a verify check is performed to confirm that the value is set to 1.And the result MB_MODE is 1.When the power is turned on again after t...

MMoro.4 by Associate II
  • 1000 Views
  • 3 replies
  • 0 kudos

Resolved! ST25DV: Area access limitations over I2C?

We are using Area 1 for a 32 byte header, and Area 2 is being used as general EEPROM storage (ENDA1 = 0x00, ENDA2=ENDA3=ENDA4=0x0F). When I setup the system ENDAx registers like this and I try to do a read across the Area1-Area2 boundary the first ...

CBarn.1 by Associate II
  • 842 Views
  • 1 replies
  • 1 kudos