NanoEdge AI Studio for non STM32 MCU
Hi, can I use NanoEdge AI Studio to make machine learning library that runs on sensor ISPU but using non STM32 MCU?Thanks.
Hi, can I use NanoEdge AI Studio to make machine learning library that runs on sensor ISPU but using non STM32 MCU?Thanks.
Hello,how can I reset FIFO_Get_Rotation_Vector in LSM6DSV16x sensor? Regards,Fehmi.
Hello, I try to write the sensor_fusion.code in ESP32. I get below compilation error;Compilation error: 'LSM6DSV16X_SFLP_GYROSCOPE_BIAS_TAG' was not declared in this scope here is my code;#include <Arduino.h>#include "lsm6dsv16x_reg.h"#include "lsm6...
Hello,I am working on sensor fusion of LSM303AGR MEMS accelerometer, As a simple program to read acceleration values, I used the I2C read and write blocks, here is my step by step: Initialize sensor: I2C write (0x32), write 0x57 on CTRL_REG1_A(0x20) ...
Hello,Has anyone worked with LSM303AGR sensor in Simulink. I am trying to interface the sensor and update values continously from board in simulink displays. I have been tryin to set up the connection for so long but nothing seems to be working and I...
Hello,Does the AlgoBuiler GUI support STEVAL-MKI109V3 hardware?
Hello,I am looking to use the LSM6DSV16x sensor for position and velocity control. What is the most effective way to achieve the best results? How can I utilize FSM, MLC, and sensor fusion to optimize performance?To clarify, the purposes are:- Trajec...
Hello,After reading the FSM document, I was unable to locate any details on uploading and processing input data for FSM configuration. Could you provide me with more information on this topic?
Hello,Can we utilize any kind of external sensors such as optical flow or range sensors, in addition to a magnetometer or pressure sensor?
Hello,Could you please provide guidance on utilizing LSM6DSV as both a master and a slave in sensor hub mode simultaneously? Kindly refer to the attached image.