Edge AI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Unicleo-GUI not Detecting my NUCLEO-IKS01A3 Board

Hi all, I installed Unicleo-GUI on my Windows laptop, and was able to read sensor data from my NUCLEO-IKS01A3 board successfully. The board was automatically identified by the software as being connected to COM4 yesterday. For some reason today the s...

Resolved! VL53L5CX as an external sensor in lsm6dsv16x

Hello, Hello,I plan to use the VL53L5CX ToF sensor in the machine learning core in lsm6dsv16x. is it possible to use the VL53L5CX  as en external sensor instead of magnetometer. Besides, may I use two external sensor in machine learning core( one wil...

FKara.3 by Senior
  • 804 Views
  • 4 replies
  • 2 kudos

LSM303AGR initialization in simulink

Hello,I am working on sensor fusion of LSM303AGR MEMS accelerometer, As a simple program to read acceleration values, I used the I2C read and write blocks, here is my step by step: Initialize sensor: I2C write (0x32), write 0x57 on CTRL_REG1_A(0x20) ...

sanathhere_1-1694771482210.png sanathhere_0-1694771156390.png

LSM303AGR Sensor in Simulink not working

Hello,Has anyone worked with LSM303AGR sensor in Simulink. I am trying to interface the sensor and update values continously from board in simulink displays. I have been tryin to set up the connection for so long but nothing seems to be working and I...

FP-IND-PREDMNT1 wi-fi connection error

Hello I have STEVAL-STWINKT1B device. When i try to connect wifi with tera term it gives this error:platform_init L#234 The network interface can not be startedany advice?

bcryhun by Associate II
  • 621 Views
  • 3 replies
  • 0 kudos

MLC Output Delay

Hello,I have recently conducted a test on the activity recognition task using the ST library with ESP32 MCU. Although it functions correctly, there are noticeable delays before action recognition occurs. I am seeking advice on how to address this iss...

FKara.3 by Senior
  • 332 Views
  • 1 replies
  • 0 kudos