Edge AI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Air Gesture Recognition using IMU

I want to implement air gesture recognition using accelerometer and gyroscope data. With different movements you should be able to make settings on the handheld device. Movements to be recognized are, for example, tipping twice or moving up and down ...

Pointes by Associate II
  • 3655 Views
  • 13 replies
  • 1 kudos

Algobuilder GUI sensortilebox

Good morning everyone, I am trying to follow the example for machine learning given for the SensorTile Boxhttps://github.com/STMicroelectronics/STMems_Machine_Learning_Core/tree/master/configuration_examples/example_2_sensortilebox_algobuilder_unicow...

Frabbit_0-1716986655732.png Frabbit_1-1716986682155.png Frabbit_2-1716986782075.png
Frabbit by Associate III
  • 365 Views
  • 1 replies
  • 0 kudos

Resolved! Using STM's IMU with non-STM32 processors

I would like to use LSM6DSOX with a linux board or potentially another micro controller.  What problems would i run into that using a stm32 couldn't have. I see there's a lot of code generation for stm32 chips. 

BA_ by Associate II
  • 834 Views
  • 4 replies
  • 3 kudos

Sensortile.box Machine learing with Unico GUI

Hello everyone,I'm trying to use the sensortile box pro for an ML alghoritm.My idea is to have a machine learning algorithm that can identify two types of vibrations: correct and fault.Using the firmware loaded on the Sensortilebox Pro Datalog 2.1.1,...

Frabbit_2-1716820083837.png Frabbit_0-1716819924874.png Frabbit_3-1716820168003.png Frabbit_4-1716820228315.png
Frabbit by Associate III
  • 2290 Views
  • 7 replies
  • 0 kudos

Resolved! [IMU] Talking to sensors on sensor hub

So i have a LSM6DSOX and connected to its sensor hub LIS3MDL. Currently I'm trying to log data to feed into the NanoEdge studio.  So i need to grab data from the actual LIS3MDL. On the sensor hub you can read and write registers through the sensor hu...

BA_ by Associate II
  • 696 Views
  • 4 replies
  • 0 kudos

LIS2DUX12 accelerometer

hi I want to start with LIS2DUX12 accelerometer programming ,It is not clear for me from where should I start . could anyone please tell me what I should do ? Regards

S1 by Associate II
  • 346 Views
  • 1 replies
  • 0 kudos

Resolved! MEMS Studio Zero Crossing

Hello everybody, We are currently evaluating the MLC of the LSM6DSOX and have a couple of general questions regarding feature calculation in MEMS Studio.I've included excerpts from the application note for quick reference. Zero-Crossing:"The feature ...

luik by Associate II
  • 469 Views
  • 1 replies
  • 2 kudos