Edge AI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Sensortile.box Machine learing with Unico GUI

Hello everyone,I'm trying to use the sensortile box pro for an ML alghoritm.My idea is to have a machine learning algorithm that can identify two types of vibrations: correct and fault.Using the firmware loaded on the Sensortilebox Pro Datalog 2.1.1,...

Frabbit_2-1716820083837.png Frabbit_0-1716819924874.png Frabbit_3-1716820168003.png Frabbit_4-1716820228315.png
Frabbit by Associate III
  • 1532 Views
  • 7 replies
  • 0 kudos

Wearable with LSM6DSMTR

 Could someone provide insights on how to identify the following user actions using a wearable integrated with LSM6DSMTR:Distinguishing between lying down, sitting, and standing.Tracking step count.Detecting if the user is walking on an incline or st...

ahboyboy by Associate
  • 298 Views
  • 2 replies
  • 1 kudos

Resolved! Unicleo-GUI not Detecting my NUCLEO-IKS01A3 Board

Hi all, I installed Unicleo-GUI on my Windows laptop, and was able to read sensor data from my NUCLEO-IKS01A3 board successfully. The board was automatically identified by the software as being connected to COM4 yesterday. For some reason today the s...

Resolved! Air Gesture Recognition using IMU

I want to implement air gesture recognition using accelerometer and gyroscope data. With different movements you should be able to make settings on the handheld device. Movements to be recognized are, for example, tipping twice or moving up and down ...

Pointes by Associate II
  • 2841 Views
  • 11 replies
  • 1 kudos

STEVAL-MKI227KA WHO_AM_I Register Value does not match

I am trying to use Unico 9.14.6.0 to get the evaluation module to work for the LSM6DSV16X.But I am getting an error that says it's an unexpected device based on the WHO_AM_I register.STEVAL-MKI109V3 updated to v3.48.3STEVAL-MKI227KA (Labeled STEVAL-M...

SCR-20230710-mlqq.png

Calibrating LSM6DSOX in arduino nano rp2040

Hello,I am doing a project for fall detectino using the MLC in the LSM6DSOX. However, i noticed that the output of the sensor for the accelerometer show values on the 1000 mg range for the z axis. I would like to calibrate the sensro but the only way...

SRodr.4 by Associate II
  • 604 Views
  • 2 replies
  • 0 kudos