Validation of depp learning model
How to input validation image dataset in the stm32cubeMX.
How to input validation image dataset in the stm32cubeMX.
How to figure out which model can be deployed on the board, according to the available RAM on the board.The ST-yolo-LC model from the ST model zoo seems to fit the board's RAM availability,(i) is it possible to train this model for my own usecase i.e...
Hello, im trying the examples from Fp-ai-facerec but it only have binaries files, so i could'nt understant how it work to config. PLease if anyone have code of this packs please dm me, thanks a lot :3
Hello,I have STM32H7S78-DK board and its have ARM cortex M7 core. As per research I saw that AI model is work on the same M7 cortex but I didn't know how it will work? would you please let us know STM32H7S78 supports AI model implements or not and if...
Hi,I'm encountering an issue while porting a trained TensorFlow-Lite model, obtained from a research paper, onto a NUCLEO-F401RE board. The process goes smoothly when analyzing and validating the code on my desktop, generating the code, and downloadi...
Hello, I am developing a Dog Activity Recognition app with CubeAI on STM32WB55 usign AI Core 9.0.0. So far, I have been following https://wiki.st.com/stm32mcu/wiki/AI:How_to_perform_motion_sensing_on_STM32L4_IoTnode . I am using the same sensor and O...
I'm currently in the process of choosing an IMU/sensor hub for activity recognition, and am stuck between the ISM330IS(N) and the ISM330DHCX. I want to use the sensor hub function and link external sensors, and run (H)AR algorithms on the IMU itself ...
Hello everyoneI hope someone can help meI have an ML model that consists of 2 inputs as shown in the picture. Is the code for the inputs correct? float ML_input[WINDOW_SIZE*NUM_POINTS]; float Diff_input[WINDOW_SIZE*NUM_POINTS - NUM_POINTS]; static ...
I came across a weird issue when using cube-x-ai. When function ai_network_run() was called, almost everything except ai_output[] in the RAM become messed up, including global variables, static and extern variables. All the peripherals need to be re-...