cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSV16X Sensor Fusion Reset

FKara.3
Senior

Hello,

how can I reset FIFO_Get_Rotation_Vector in LSM6DSV16x sensor?

 

Regards,

Fehmi.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Ciao @FKara.3 ,

Can you write me the register name and the bit you are referring to?

Thanks

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Federica Bossi
ST Employee

Ciao @FKara.3 ,

Can you write me the register name and the bit you are referring to?

Thanks

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
FKara.3
Senior

Ciao @Federica Bossi ,

/*
@file LSM6DSV16X_Sensor_Fusion.ino
@author STMicroelectronics
@brief Example to use the LSM6DSV16X library with Sensor Fusion Low Power.
*******************************************************************************
Copyright (c) 2022, STMicroelectronics
All rights reserved.

This software component is licensed by ST under BSD 3-Clause license,
the "License"; You may not use this file except in compliance with the
License. You may obtain a copy of the License at:
opensource.org/licenses/BSD-3-Clause

*******************************************************************************
*/
#include <LSM6DSV16XSensor.h>

#define ALGO_FREQ 120U /* Algorithm frequency 120Hz */
#define ALGO_PERIOD (1000U / ALGO_FREQ) /* Algorithm period [ms] */
unsigned long startTime, elapsedTime;

LSM6DSV16XSensor AccGyr(&Wire);
uint8_t status = 0;
uint8_t tag = 0;
float quaternions[4]={0};

void setup() {

Serial.begin(115200);
while (!Serial) yield();

Wire.begin();
// Initialize LSM6DSV16X.
AccGyr.begin();

// Enable Sensor Fusion
status |= AccGyr.Enable_Rotation_Vector();

if(status != LSM6DSV16X_OK) {
Serial.println("LSM6DSV16X Sensor failed to init/configure");
while(1);
}
Serial.println("LSM6DSV16X SFLP Demo");
}

void loop() {
uint16_t fifo_samples;
// Get start time of loop cycle
startTime = millis();
// Check the number of samples inside FIFO
if(AccGyr.FIFO_Get_Num_Samples(&fifo_samples) != LSM6DSV16X_OK){
Serial.println("LSM6DSV16X Sensor failed to get number of samples inside FIFO");
while(1);
}

// Read the FIFO if there is one stored sample
if (fifo_samples > 0) {
for (int i = 0; i < fifo_samples; i++) {
AccGyr.FIFO_Get_Tag(&tag);
if(tag==0x13u){
AccGyr.FIFO_Get_Rotation_Vector(&quaternions[0]);

// Print Quaternion data
Serial.print("Quaternion: ");
Serial.print(quaternions[3], 4);
Serial.print(", ");
Serial.print(-quaternions[1], 4);
Serial.print(", ");
Serial.print(quaternions[0], 4);
Serial.print(", ");
Serial.println(quaternions[2], 4);

// Compute the elapsed time within loop cycle and wait
elapsedTime = millis() - startTime;
delay(ALGO_PERIOD - elapsedTime);
}
}
}
}


Previously, I was reading quaternion values from FIFO but now I can't because fifo_samples shows 0.

 

Regards,

Fehmi