Edge AI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Air Gesture Recognition using IMU

I want to implement air gesture recognition using accelerometer and gyroscope data. With different movements you should be able to make settings on the handheld device. Movements to be recognized are, for example, tipping twice or moving up and down ...

Pointes by Associate II
  • 5571 Views
  • 13 replies
  • 1 kudos

Algobuilder GUI sensortilebox

Good morning everyone, I am trying to follow the example for machine learning given for the SensorTile Boxhttps://github.com/STMicroelectronics/STMems_Machine_Learning_Core/tree/master/configuration_examples/example_2_sensortilebox_algobuilder_unicow...

Frabbit_0-1716986655732.png Frabbit_1-1716986682155.png Frabbit_2-1716986782075.png
Frabbit by Associate III
  • 573 Views
  • 1 replies
  • 0 kudos

Resolved! Using STM's IMU with non-STM32 processors

I would like to use LSM6DSOX with a linux board or potentially another micro controller.  What problems would i run into that using a stm32 couldn't have. I see there's a lot of code generation for stm32 chips. 

BA_ by Associate II
  • 1458 Views
  • 4 replies
  • 3 kudos

Sensortile.box Machine learing with Unico GUI

Hello everyone,I'm trying to use the sensortile box pro for an ML alghoritm.My idea is to have a machine learning algorithm that can identify two types of vibrations: correct and fault.Using the firmware loaded on the Sensortilebox Pro Datalog 2.1.1,...

Frabbit_2-1716820083837.png Frabbit_0-1716819924874.png Frabbit_3-1716820168003.png Frabbit_4-1716820228315.png
Frabbit by Associate III
  • 6393 Views
  • 7 replies
  • 0 kudos

Resolved! [IMU] Talking to sensors on sensor hub

So i have a LSM6DSOX and connected to its sensor hub LIS3MDL. Currently I'm trying to log data to feed into the NanoEdge studio.  So i need to grab data from the actual LIS3MDL. On the sensor hub you can read and write registers through the sensor hu...

BA_ by Associate II
  • 2153 Views
  • 4 replies
  • 0 kudos

Wearable with LSM6DSMTR

 Could someone provide insights on how to identify the following user actions using a wearable integrated with LSM6DSMTR:Distinguishing between lying down, sitting, and standing.Tracking step count.Detecting if the user is walking on an incline or st...

ahboyboy by Associate
  • 737 Views
  • 2 replies
  • 1 kudos

Resolved! ISM330DHCX FSM Change DECTREE Value for CHKDT condition

Hi,I am trying to use the FSM of the ISM330DHCX to check multiple decision tree outputs from the MLC.I want to be able to change the Decision Tree value in the CHKDT condition within the program flow, as I want to be checking multiple decision trees ...

Resolved! Decision Tree evaluation Parameters in LSM6DSV16x

Hello, I have a question regarding the evaluation parameters for decision tree results. As you can see in the picture below, the Mean Absolute Error and Root Mean Squared Error are high, but the accuracy is also high. I am confused because I thought ...

FKara3_0-1708462905883.png
FKara.3 by Senior
  • 871 Views
  • 2 replies
  • 1 kudos