Edge AI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Gain setting for microphones on STWINKT1B

Hi guys I have a couple of questions. I've been using the microphones on STWINKT1B to record some events for about a month now. I've utilized both the FP-SNS-DATALOG1 and FP-SNS-DATALOG2 firmware for data logging. While the digital mic (imp34dt05) de...

Resolved! NanoEdgeAIStudio : is it possible to log ultrasounds ? (STWINKT1B)

Hi, I am using NanoEdgeAIStudio to detect anomalies on microphone signal. I am particularly interested in logging ultrasounds (from 20kHz to 100kHz). I used the Datalogger tool (in NanoEdgeAIStudio) to set up the datalogger and generate the neai_data...

anthonyADV_1-1706803687465.png anthonyADV_2-1706804921863.png

LSM303AGR Sensor in Simulink not working

Hello,Has anyone worked with LSM303AGR sensor in Simulink. I am trying to interface the sensor and update values continously from board in simulink displays. I have been tryin to set up the connection for so long but nothing seems to be working and I...

STWINKT1B Cloud Streaming and Predictive Maintenance

I am looking for a solution for a cohesive predictive maintenance application using continuous, real-time streaming of data that is continuously monitored for any changes. I was looking to use the industrial grade digital MEMS microphone (IMP34DT05),...

alars1 by Associate
  • 838 Views
  • 2 replies
  • 0 kudos

FP-IND-PREDMNT1 wi-fi connection error

Hello I have STEVAL-STWINKT1B device. When i try to connect wifi with tera term it gives this error:platform_init L#234 The network interface can not be startedany advice?

bcryhun by Associate II
  • 761 Views
  • 3 replies
  • 0 kudos

Resolved! Detection of unwanted noise in cars (Sensortile.box)

I'm trying to do a program like a baby crying and i'm looking for the code of babycrying program. I need to do a program that detects unwanted noises in cars, so i think that maybe is similar than the babycrying app.I thought it was possible using th...

SAbba.1 by Associate III
  • 1255 Views
  • 5 replies
  • 1 kudos