LSTM
Hello,What is the solution for implementing an LSTM model on an STM32?
Hello,What is the solution for implementing an LSTM model on an STM32?
Does anyone knows how to open the .ioc file of Image classification example from Model Zoo? Where is the location of this ioc file as I couldn't found it and is there anyway for me to obtain the ioc file? Thanks
Board - B-L4S5I-IOT01A BoardAI application tool - edgeimpulseIDE - STM32CubeIDE 1.15.11. AI model generated from edge impulse AI platform for B-L4S5I-IOT01A Board. Package downloaded.2. CUBE mx generate code for B-L4S5I-IOT01A Board.3. Edge-Impulse ...
My binary classification algorithm has one input (270 data) and one output, I refer to section 6.4 of the code(AI:How to perform motion sensing on STM32L4 IoTnode - stm32mcu (stmicroelectronics.cn))Question 1:but the output category is always wrong, ...
When I use a function 【int ai_run(const void *in_data, void *out_data)】to make predictions,the out_data always output【0】No matter how I change the value of the input data, the value of the output data will not change, it will always be 0.int ai_run(c...
Can I run a Machine Learning model using Tensor flow lite or Edge Impulse on STM32F103C8T6 with 64kb flash.Actually I don't have any choice but to try to run the ML model on Blue pill, because my there is unavailability of other MCU boards at the ins...
My binary classification algorithm has one input (270 data) and one output, I refer to section 6.4 of the code(AI:How to perform motion sensing on STM32L4 IoTnode - stm32mcu (stmicroelectronics.cn))but the output category is always wrong, I don't kno...
I am trying to deploy an AI model on an MCU using Cube AI TFLite Micro runtime. The model is successfully flashed but I get the following error when the validation starts:[AI:network] stm32ai: error: argument --mode: invalid choice: 'stm32_io_only' (...
..\..\AI\X-CUBE-AI\App\app_x-cube-ai.c(93):error: #20: identifier "AI_AI_DATA_ACTIVATION_1_SIZE" is undefinedstatic uint8_t poo10[AI_AI_DATA_ACTIVATION_1_SIZE];...\...\AI\X-CUBE-AI\App\app_x-cube-ai.c(95): error: #28: expression must have a constant ...
Thank you!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!The error are:TEMPLATE - initializationTEMPLATE - Error (ai_network_create_and_init) - type=0x33 code=0x41 and I also have another issue is when I using .h5 file to g...