The error occurs when I try to run the code generated for model squeezenetv1.1_xxx_tfs_int8.tflite The command I used to generate code is stm32ai generate -m squeezenetv1.1_128_tfs_int8.tflite -O ramAnd I follow the guide "How to run locally a c-mode...
The error occurs in both Mac m1 and windows. When I use "stm32ai validate/generate" command, I find that "-O ram" outputs totally strange results. Let's use fdmobilenet_0.25_224_tfs_int8.tflite from stm32ai-modelzoo as an example. "stm32ai validate -...
I am trying to deploy an AI model on an MCU using Cube AI TFLite Micro runtime. The model is successfully flashed but I get the following error when the validation starts:[AI:network] stm32ai: error: argument --mode: invalid choice: 'stm32_io_only' (...
In the STM32Cube.AI workshop - 6 Neural Network (NN) Model creation - YouTube, tutacousticscenes2016 does not work. librosa returns an error message: ModuleNotFoundError: No module named '_soundfile_data'. Please suggest a workaround.
I encountered an error while analyzing an ONNX model quantized with int8, and I'm unsure how to resolve it. Is there any technical support available to assist me with this issue?
Here are the software versions I'm using:STM32CubeMx - 6.3.0MCU package for STM32H7 - 1.9.0X-CUBE-AI - 7.0.0MCU - STM32H743ZITxIAR EW for ARM - 8.40.1I run into this problem since I have added the X-CUBE-AI software pack. every time I open the X-CUBE...
With a fresh installation of STM32CubeIDE 1.6.1 on a clean WIndows 10 Pro 20H2, after adding X-CUBE-AI 6.0.0 to a new STM32 project, Analyze fails with:ImportError: cannot import name 'get_all_providers' from 'onnxruntime.capi._pybind_state' (C:\User...