Edge AI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Invalid Initializer error with auto-generated code X-CUBE-AI

Hello!I'm having the exact same issue than the one described here: https://community.st.com/s/question/0D53W00001YbCCCSA3/invalid-initializer-and-initializer-element-is-not-constant-errors-in-stmcubeai?t=1662110397892Wrapping ai_network_params inside...

C. Mart by Associate III
  • 2515 Views
  • 5 replies
  • 1 kudos

No source available for "ai_platform_network_process() at 0x8xxxxx"

Hi,We are trying a very simple deep neural network model with 20 inputs and 3 outputs and want to generate inferences in real-time. We are following the instructions from the document "Getting started with X-CUBE-AI Expansion Package for Artificial I...

PGaja.1 by Associate II
  • 3050 Views
  • 16 replies
  • 4 kudos

Resolved! STM32CubeIDE does not emit the X-CUBE-AI middleware

I am using STM32CubeIDE v1.12.1 on macOS. I have noticed that, when I import a project generated with STM32Cube.AI Developer Cloud, whenever I open the IOC and make a change to the device configuration that requires to regenerate the code, the projec...

PB1 by Associate III
  • 5833 Views
  • 16 replies
  • 2 kudos

How to implement YOLO on STM32 H7

Hello,I'm sorry that these are in fact many questions but I'm wondering why I can't analyse any of the ONNX models that I've downloaded. I tryied YOLOv8n (12MB), YOLOv6n (18MB), YOLOv5su (36MB), YOLOv4tiny (24MB) and YOLOv2 (62 MB) and none of these ...

CRAHI.1 by Associate
  • 5932 Views
  • 5 replies
  • 0 kudos

error when analyzing the .onnx model in stm32cubeMX by stm32cube.AI

Hi, Thanks for your attention. I am analyzing the .onnx format model but an error occurs. I try to reinstall the stm32cubeMX but it doesn't help. The part of architecture is: Here is the log information. Can you help me with this problem? @Romain LE ...

0693W00000QKl99QAD.png 0693W00000QKlBZQA1.png
BHuan.3 by Associate III
  • 5412 Views
  • 9 replies
  • 1 kudos