Resolved! How to use NanoEdge AI-generated files in keil
Can NanoEdge AI only generate.a static library? If so, how do I use it in keil? This is because keil does not use GCC but ARMCC.
Can NanoEdge AI only generate.a static library? If so, how do I use it in keil? This is because keil does not use GCC but ARMCC.
Hi,I have managed to program the STM32F746G-DISCO with a simple neural network but when I try to do it using the external Flash by using the option in advanced settings (External NOR Flash) it doesn't work. Any idea why? Is there anything else I need...
Hello,I am using CubeMX 5.1.0 with the X-CUBE-AI 3.4 package. It works really fine with Atollic TrueStudio and the GCC. However, the perfomance / runtime of our algorithm is not satisfactory, so that we would like to use the ARM Compiler 6.12 to look...