Edge AI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

B-U585I-IOT02A Board AI application with external Flash and RAM

Hello,I want to deploy a AI model on B-U585I-IOT02A board. I'm using the X-Cube-AI plugin for that. Since my model is not able to run on internal flash and RAM, I have selected to use external FLASH and SRAM (from advanced settings in X-Cube-AI). The...

MJog.1 by Associate II
  • 1426 Views
  • 3 replies
  • 2 kudos

Resolved! How to change RAM limits on X-Cube AI for a dual core MCU.

I am using a STM32WL55JC2 Nucleo Board that mounts a dual core M4/M0+, I changed the linker script in order to have more RAM and FLASH on the M4, but this change is not reflected on the X-CUBE AI interface when adding a new network.Is it possible to ...

LMain.1 by Associate II
  • 1371 Views
  • 4 replies
  • 0 kudos

Resolved! How to use external Flash with STM32Cube.AI?

Hi,I have managed to program the STM32F746G-DISCO with a simple neural network but when I try to do it using the external Flash by using the option in advanced settings (External NOR Flash) it doesn't work. Any idea why? Is there anything else I need...

DPast.2 by Associate
  • 1164 Views
  • 2 replies
  • 0 kudos

[AI:network] Error flashing firmware after building successfully

I was using NUCLEO-L476RG.When I tried to validate on target, I can build successfully but the message below showed up.How can I do?​​===========================update=========================I found that the rom size seemed to be too large. Maybe it...

0690X00000Bvns0QAB.jpg 0690X00000BvnvsQAB.jpg 0690X00000BvnzzQAB.jpg 0690X00000Bvo70QAB.jpg