Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

download.spc5studio.com

Core 1.3.0, Contrib 1.3.0 and RLA 1.6.0 Released The new main update site http://download.spc5studio.com/updates/ has been updated with Core, Contrib and RLASW Prerequisite : SPC5Studio 5.8.1New or updated componentsCore 1.3.0Enhanced dynamic propert...

How do I enable I/O settings in the board initialization component for my SPC58 discovery kit project in SPC5 Studio?

When I import example projects for my SPC58 board, I am able to edit the I/O settings. Specifically, I can change the I/O mode of GPIO pins to be input or output instead of both, which I can't do from the Pin Map editor. But when I try and select thi...

Is there a document describing how to modify different configurations in SPC5Studio? I need to select different .ld files depending on the configuration.

 I am asking because I created a second configuration (Now I have the " Default" and the "Release"). My goal is to find a way to force the linker to use one .ld file with the " Default" configuration and another .ld file with the "Release" configurat...

Resolved! BSDL Files for SPC56

Posted on October 27, 2014 at 12:00Hello!I am looking for the BSDL files for the SPC56 family microcontrollers.Does anyone knows if they are available or the link to download them?Thanks #spc56

Dual Core Initialization

I am working on Dual Core SPC58x Series and I face some trouble with Dual core initialization and Usage.For the Moment it will be very much helpful if you can share a document / Application Note / Example on the Initialization and Usage of Dual Core ...

spc5 studio can't detect my board

Good morningWe connected the board spc570 by microUSB, our operating system (both windows 7 and windows 10) detected it as "SPC570S-DISP discovery board" but can't install any driver. We have already downloaded and installed SPC5 studio with "comple...

TGecc by Associate
  • 1214 Views
  • 1 replies
  • 0 kudos