Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Setup for SPC58xG Core0 and Core2

Hello Community,my application is already running on CORE2, but i want activate the Core0 and let my application  on Core0. Do you have an example how to Setup the Dual core0 and 2?Thank you in advanceTam​

Wakeup SPC570S40E1 from STOP mode by NMI pin.

Posted on May 31, 2018 at 09:31 Hello everyone; I am working with SPC570S discovery board. I would like to implement the STOP mode to reduce the power consumption and then wake up by using NMI pin like PA[4] or PC[15]. I already entry the STOP ...

0690X0000060L2KQAU.png 0690X0000060L2PQAU.png
Tran Hung by Associate II
  • 5589 Views
  • 11 replies
  • 0 kudos

download.spc5studio.com

 GTM 1.7.0 Released The new main update site http://download.spc5studio.com/updates/ has been updated with GTM 1.7.0.SW Prerequisite : SPC5Studio 5.8.1GTM 1.7.0Improved ATOM, TBU, DPLL and CMU support MCS compiler plugin integrated to easy MCS code c...

How to add Runtime IO component to an existing project?

I recently downloading the update for runtime IO component on SPC5studio, however, I cannot seem to find a way to add the component to either existing or new project from import wizard from the IDE gui.

fm by Associate II
  • 1239 Views
  • 1 replies
  • 0 kudos

UART Rx interrupt on SPC560D

SPC5 Studio for SPC560D-DIS board, LINFLEX0 configured as UART, Tx is okay but Rx ISR is not getting called. I am using the auto generated Serial Test application which creates IRQ handlers in "spc5_linflex.c". I have break points set in both Tx and ...

fm by Associate II
  • 1241 Views
  • 1 replies
  • 0 kudos

Problem with ADC on the Bernina

Hello,I've got a problem with max analog channel input voltage. When all supply voltages are 5V everything is fine. But if VDD_HV_IO_MAIN voltage is 3.3V while VDD_HV_ADV is 5V, the analog channel input voltage becomes limited over 4V. This problem i...