User Activity

Posted on November 27, 2017 at 03:45 I need to update the SPC5 4.0 project to SPC5 5.6 project. But there is no SPC560Pxx IRQ component RLA in SPC5 5.6.
Posted on November 27, 2017 at 01:24I use the SPC5 Studio 5.6 to open an old project and get the following error.08:20:06 **** Build of configuration Default for project BZW111A_CAT_MHE_Gamma ****make all Compiler Optionsppc-freevle-eabi-gcc -c -mcp...
Posted on November 15, 2017 at 01:32 PIT registers are accessible only when the core is in supervisor mode. How to go to the supervisor mode?
Posted on November 06, 2017 at 01:37After MCU reset, I got the following and the IOT bit is set. But according to the RM0046(Reference manual, September 2013, Rev 5) the IOT bit should be reset after MCU reset.#lintcsr
Posted on October 26, 2017 at 09:07How could I read out the hex file from SPC560P34L1CEFA?#hex