2017-12-13 7:45 AM
Dear All ,
SPC5Studio 5.7.0 is available
*** Highlights ***
Here are the changes coming with SPC5Studio v5.7
For Mass Market:
===========
- Windriver support (see application level)
- minor bugs fixing
For Selected Customers:
================
- Chorus 2M starter kit and additional drivers:
CAN, Serial, PIT, STM, SPI, SWT FLASH
- Eiger starter kit
- Power Consumption wizard
Low power mode
- ILi9341 middleware
Use these following update sites :
http://spc5.drive.cloudforge.com/projects/spc5releases/SPC5Studio/updates5
(New update Site for free GCC feature and PLS Feature) (Hightec compiler)#spc5studio #spc58 #spc57 #spc56