STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP157C gnu toolchain

Hi,I would like to compile with the GNU toolchain directly on the device, without the use of cross-compilation. it's possible?In which way can i do that?

PFran.17 by Associate II
  • 593 Views
  • 1 replies
  • 0 kudos

Resolved! Let's Get Started - Garbage Serial Terminal Output

Hi,I've been following the guide over at:https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157C-DK2/Let%27s_start/Execute_basic_commandsI'm using a Windows 10 as a host, but I was hoping I'm not the only one. I don't have acces...

TOlli by Senior
  • 1430 Views
  • 2 replies
  • 0 kudos

STM32MP157-DK2 Ethernet

Hi, I can't to connect my board by ethernet connector, when I connect the cable both leds are always off. I try using ifconfig to set a ip but my board doesn't respond to ping request, but when I used ifconfig to set ip over usb0 my board respond to ...

ECaba by Associate II
  • 873 Views
  • 2 replies
  • 0 kudos

Can't Debug in Engineering Mode using STM32MP157-DK2. OpenOCD Error: Could not find MEM-AP to control the core

Trying to create a simple application that will toggle LD9 in Engineering Mode but get an error with the OpenOCD.Output on console window is as follows:Open On-Chip Debugger 0.10.0+dev-01124-gbfb41e6 (2018-11-16-15:23) Licensed under GNU GPL v2 For b...

BMcCa.3 by Associate II
  • 1314 Views
  • 3 replies
  • 0 kudos

Resolved! The new ANA0 / ANA1 pins

Hi,I'm currently figuring out about the new ANA0 / ANA1 pins.As far as I understand, those pins are always connected to the ADC so that I don't need to touch the GPIO registers in order to use those pins. Is my understanding correct?Also I can connec...

0690X000009Ymq4QAC.png

STM32MP157-DK2 not connecting to ethernet

Hello,i have a problem when tring to establish a ethernet connection with the STM32MP157-DK2 board.Windows 10 -64bit system, no firewall, no antivirus. DHCP enabled.Tried with cross & straight CAT6 ethernet cable.I cannot establish a SSH connection...

Bogdan by Senior
  • 2023 Views
  • 8 replies
  • 0 kudos

Resolved! Slightly confused about IPCC peripheral

I have a STM32MP157C-DK2, and I'm interested in better understanding how the IPCC peripheral works. I've tried out the OpenAMP echo example and trawled through its code, and the associated HAL code. I have generally completely avoided the HAL for mic...

unicycle by Associate III
  • 769 Views
  • 1 replies
  • 0 kudos

Resolved! Possible bugs found in STM32CubeMP1 & misleading AN5253.

Hi,I'm currently working on porting Arduino Core for STM32 to STM32MP1 Cortex M4 core.Here are some stuff I found:Typo: I post it in the Github: https://github.com/STMicroelectronics/STM32CubeMP1/pull/1Possible bugs in HAL driver: stm32mp1xx_hal_conf...

STM32MP1 shared memories allocation

Hi,i am trying to understand where and how are RETRAM, MCUSRAM, virtio ring buffer descriptors and virtio buffers allocated. In the next link:https://wiki.st.com/stm32mpu/wiki/Linux_remoteproc_framework_overviewIt is described the device tree configu...

ALibe by Associate
  • 725 Views
  • 1 replies
  • 0 kudos