cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157-DK2 Ethernet

ECaba
Associate II

Hi, I can't to connect my board by ethernet connector, when I connect the cable both leds are always off. I try using ifconfig to set a ip but my board doesn't respond to ping request, but when I used ifconfig to set ip over usb0 my board respond to ping and I can copy the hello_world example.

Is my ethernet interface damaged? or I need to do other configuration?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi,

Did you try a point to point connection or through LAN/DHCP ?

Thx

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
ECaba
Associate II

Hello, I followed the link: https://wiki.st.com/stm32mpu/wiki/Ifconfig, and I use: ifconfig eth0 up, next: ifconfig eth0 192.168.1.40 and I my board respond to ping request but my ethernet connector leds are always off.