STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP157C-DK2 Bluetooth mesh

I have a STM32MP157C-DK2 eval kit and am looking into Bluetooth mesh. According to Murata the wireless \ bluetooth module that contains a Cypress part is mesh compliant and the board has v5.50 of BlueZ so theoretically the version of Linux supports i...

RichM1 by Associate
  • 907 Views
  • 1 replies
  • 0 kudos

Resolved! a loop which iterates infinitely for x seconds - stm32mp157c-dk2

Hi,In my M4 program within while loop, I have made a for loop which iterates infinitely for 0.75 seconds like this but didnt work at all. I used time.h for that. Are we allowed to make this kind of loop within the while loop in M4 program ?Do you hav...

IYetk by Associate III
  • 1285 Views
  • 6 replies
  • 0 kudos

MIPI DSI display flicking at 1280x720@60

 Dear team,We have a design with stm32mp157aac MPU, and we use MIPI DSI as the display interface to a device with 1280x720@60 RGB888, the PCLK is 74.25MHz, the DSI works at non-burst sync event video mode. But the image is flickering continously. Whe...

0690X000009jHOQQA2.jpg
SunnyGeGe by Associate III
  • 1769 Views
  • 4 replies
  • 1 kudos

Error when using plasma-mobile in openstlinux-x11

Hi there,I am trying to use the plasma-mobile enviroment as default in the x11 distro. I documented in detail everything in this issue (easy to reproduce): https://github.com/schnitzeltony/meta-qt5-extra/issues/73Can someone from ST look into this to...

VBurs by Associate II
  • 511 Views
  • 0 replies
  • 0 kudos

How to improve the USB OTG speed of STM32MP157?

The hardware is STM32MP157C-DK2 board.​1. We setup the test environment as below:​We bridge the USB port and the Ethernet port in the ST.The throughput is about 270Mbit/sec(Limited by the usb to Ethernet convertor).2. Another test environment is:The ...

0690X00000ARKbwQAH.bmp 0690X00000ARKczQAH.png
JYan.17 by Associate
  • 809 Views
  • 1 replies
  • 0 kudos