STM32 MPUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP1 - Bare metal on A7

Hi,I have a current project using the M7 that I need to port over to the A7. The goal is to be running bare-metal code on the A7, like we are on the M7. Currently, I am following this open source guide to run bare-metal on the A7 and it seems to work...

mkurtz by Associate II
  • 1090 Views
  • 6 replies
  • 0 kudos

Resolved! Witch STM32 chip for my project ?

Hi everybody!I working on a simple project but with some sensors and co.I'm newbie with the STM32 and I want to try to port the project from the ATmega2560 to the STM32.But witch chip? I need :> SPI for an TFT screen 2.2" (ILI9340C or ILI9341)> SPI f...

DMost by Associate
  • 1013 Views
  • 2 replies
  • 0 kudos

Resolved! STM32MP FMC SRAM & ARM M4

For an application we are investigating this processor and have two questions,We want to connect an external chip to the FMC bus. It is somespecialized ASIC handling some real-time communication.I don't see the option in the STM32Cube to active the F...

Resolved! Could not set DRM mode for screen DSI1/Could not queue DRM page flip on screen DSI1 (Permission denied) for st-example-image-qt

Hi,I have succesfully built a image st-example-image-qt from the DISTRO openstlinux-eglfs.I have deployed the image on sd card, and played it on STM32MP157C-DK2.System is booting without a problem, and the splashscreen was shown.Then, I tried one of ...

Resolved! DFU not detected

HiI got an STM32MP157C-DK2 during the Embedded World.But Windows7 isn't detecting the DFU ... It detects only the STLink (UART) ....Same issue in a Ubuntu-16 (which is running in VirtualBox on the same Windows 7)Any suggestion?Regards Francesco

Resolved! STM32MP1 Distribution package access rights

Hi,I'm planning to buy an STM32MP1 discovery kit (when available) and I'm wondering how to get access to the distribution package. I read on wiki.st.com that I have to request these rights to my ST support contact but I can't found out how to do it.T...

Silicio by Associate
  • 575 Views
  • 2 replies
  • 0 kudos