STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I'm not using USB nor ADC/DAC on the STM32MP157A. Can I tie VDDA, OTG_VBUS, AND VDD3V3_USBxS to circuit ground (VSS)?

If I'm interpreting Table 13 correctly (datasheet p 128), VDDA can be set to 0 volts provided VREF is not used. Similarly power pins related to USB can also be set to 0 volts. Looking in the datasheet p29,I just need to star-connect VDD_ANA, VDD_PLL...

JCond.1 by Associate II
  • 2092 Views
  • 3 replies
  • 0 kudos

Resolved! Out of order STM32MP157CAC. PANIC at PC : 0x2fff2d17 Exception mode=0x00000016 at: 0x2fff2d17

Hello.I developed my own board based on A-DK1 board using STM32MP157CAC and MicroSD, PMIC, Ethernet and DDR periphery. When I connect my plate to the usb with sd-card (st-link 2.1) I always receive the message:PANIC at PC : 0x2fff2d17Exception mode=0...

DFomi.1 by Associate II
  • 3135 Views
  • 2 replies
  • 0 kudos

Resolved! The question about STM32MP157CAC3 supply

Hello. I have used the STM32MP157A-DK1 this year and I have learned to work with it. Now I develop my own PCB with STM32MP157CAC3. There is a 12-V external power supplier in it. I do't use USB Type-C. Can I do like this? I care about pins USB_PWR_CC1...

DFomi.1 by Associate II
  • 1622 Views
  • 5 replies
  • 0 kudos

glib meson error: ERROR: <ExternalProgram 'python3' is not a valid python or it is missing setuptools

I have been trying to compile an image in Yocto with a custom machine to load my own device tree, but when trying to compile I always get the same error, here is a log: Log data follows:| DEBUG: Executing shell function do_configure| gtkdocize: neith...

FPini.1 by Associate II
  • 3346 Views
  • 7 replies
  • 0 kudos

STM32MP1 bRIGUP watchdog trip

HI. I have a custom board that basically identical to the PDKWe Made 2 Boards for test.One starts up OKThe Other failsSection of Console belowThe section of interest is the lineINFO:  CPU 0 IT Watchdog 2 and soThe Same SDCard in both.Must be a hardwa...

Bkell.1 by Associate II
  • 2660 Views
  • 3 replies
  • 0 kudos

Resolved! The problem with facilitating uboot errors

When compiling the U-boot, these four commands are used:PC $& gt; export KBUILD_OUTPUT=.. /build/stm32mp15_trustedPC $& gt; export DEVICE_TREE=stm32mp157c-dk2PC $& gt; make stm32mp15_trusted_defconfigPC $& gt; make alluse the first: export KBUILD_OUT...

Ffu.1 by Associate II
  • 2637 Views
  • 4 replies
  • 0 kudos