2021-07-28 4:11 PM
On my custom board, I configured PZ0, PZ1, PZ2 for SPI1 with device tree, and linux kernel probed successfully and populate spidev node and it works fine, but if look at debug information in /sys/kernel/debug/pinctrl/, it populate something like "pin 400 (PZ0): device 44004000.spi function analog group PZ0", I expect "AF5" for pin function instead of "analog", especailly for this case it has configured as SPI alternate pin already. Is this a kernel bug or some trick I have to do with device tree?
2021-07-28 4:23 PM
I saw samething with DK2 board also,
2021-07-29 12:55 AM
Hi,
is your Device Tree generated using CubeMx ?
Which ecosystem version are you using ?
could you please check if uboot and kernel device tree are identical ?
could you share related device tree nodes (pinctrl and spi only) ?
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.