STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Cannot get can0 interface to appear on STM32MP157f-dk2

Hello,I am trying to setup CANbus on the STM32MP157f-dk2 board, but I am unable to get any CAN interface to appear. I have installed the STM32MP1 OpenSTLinux Developer-Package onto the board, and I am using an SN65HVD230 transceiver.First I tried ena...

IanY_4-1715666366381.png IanY_5-1715666429018.png
IanY by Associate II
  • 2543 Views
  • 10 replies
  • 0 kudos

STM32MP135: U-boot - No serial driver found

I'm using minimal device tree files to get a custom (MYIR MYC-YF135) board to boot. At the moment I'm stuck when OP-TEE should give the control to u-boot. The boot stops on error message: No serial driver found   .... F/TC:0 0 _regulator_enable:150 v...

jhi by Senior
  • 2838 Views
  • 7 replies
  • 0 kudos

Resolved! How to setup FDCAN on STM32MP157F-DK2?

Hi everyone! I'm here with my devkit and trying to have FDCAN working properly! I compiled the Yocto distribution for the board and I followed all the tutorials in the wiki ( https://wiki.st.com/stm32mpu/wiki/Category:CAN ) and here's what I came up ...

SScar.2 by Senior
  • 5028 Views
  • 13 replies
  • 3 kudos

IAC exceptions when launching M33 core

Hello, I am trying to load an .elf file on the M33 core on my stm32mp257f processor. When I launch the remote core using remoteproc I get the following errors.       root@stm32mp257f-hydra-mx:~# echo -n /home/root > /sys/module/firmware_class/paramet...

ADC DMA on stm32mp257 interrupt not triggering

Hello,I am trying to get my ADC using DMA working in my freertos program running on the M33 core of the stm32mp257 processor. I set up ADC1 on HPDMA3 using cube MX see config below.I am getting a few issues.1. If I used the generated code I get a run...

nielsenni101_0-1738352115447.png

Bringing up STM32MP257 & Debug

We have built a SBC using the 257EV as a reference in Altium. We are trying to use debug. We have created a ST14 connector to connect to a STLink3 using UART 2 as the debug serial port.Is this possible, and should we use SWD or JTAG to debug the proc...

SCROGGYG by Associate
  • 443 Views
  • 1 replies
  • 0 kudos

Remoteproc fails while waiting for resources

When trying to attach to M4 upon Linux boot (autoboot=1), it fails to bind resources:Remoteproc driver attempts to probe m4 resources, but all are waiting for pinctrl@50002000 which does not appear before remoteproc probe has timed out. I can see in ...

vsaakian by Associate III
  • 290 Views
  • 0 replies
  • 0 kudos