Skip to main content
jhi
Senior
July 25, 2024
Question

STM32MP135: U-boot - No serial driver found

  • July 25, 2024
  • 7 replies
  • 4346 views

I'm using minimal device tree files to get a custom (MYIR MYC-YF135) board to boot. At the moment I'm stuck when OP-TEE should give the control to u-boot. The boot stops on error message: No serial driver found

 

 

 

....
F/TC:0 0 _regulator_enable:150 vdd
F/TC:0 0 _regulator_enable:188 vdd refcount: 1
F/TC:0 0 _regulator_enable:150 v3v3
F/TC:0 0 _regulator_enable:188 v3v3 refcount: 1
F/TC:0 0 _regulator_enable:150 vddcore
F/TC:0 0 _regulator_enable:188 vddcore refcount: 1
F/TC:0 0 regulator_core_dump:920 Dump Regulators
F/TC:0 0 regulator_core_dump:921 reg name use en mV min max flags supply
F/TC:0 0 regulator_core_dump:941 usb33 usb33 0 0 3300 3300 3300 0
F/TC:0 0 regulator_core_dump:941 reg18 reg18 0 1 1800 1800 1800 0 vdd
F/TC:0 0 regulator_core_dump:941 reg11 reg11 0 1 1100 1100 1100 0 vdd
F/TC:0 0 iod_get_voltage:115 sdmmc1_io: get volt
F/TC:0 0 iod_get_state:104 sdmmc1_io: get state
F/TC:0 0 regulator_core_dump:941 sdmmc1_i sdmmc1_i 1 1 3300 0 65535 0x1 vdd
F/TC:0 0 iod_get_voltage:115 sdmmc2_io: get volt
F/TC:0 0 iod_get_state:104 sdmmc2_io: get state
F/TC:0 0 regulator_core_dump:941 sdmmc2_i sdmmc2_i 1 1 3300 0 65535 0x1 vdd
F/TC:0 0 regulator_core_dump:941 vdd vdd 1 1 3300 3300 3300 0x1
F/TC:0 0 regulator_core_dump:941 v3v3 v3v3 1 1 3300 3300 3300 0x1
F/TC:0 0 regulator_core_dump:941 vddcore vddcore 1 1 1350 1350 1350 0x1
D/TC:0 0 call_initcalls:40 level 6 scmi_regulator_consumer_init()
F/TC:0 0 get_supply_phandle:114 voltd: supplied by 7
D/TC:0 0 scmi_regulator_consumer_init:322 scmi voltd shares reg11 (node reg11) on domain ID 0
F/TC:0 0 get_supply_phandle:114 voltd: supplied by 8
D/TC:0 0 scmi_regulator_consumer_init:322 scmi voltd shares reg18 (node reg18) on domain ID 1
F/TC:0 0 get_supply_phandle:114 voltd: supplied by 9
D/TC:0 0 scmi_regulator_consumer_init:322 scmi voltd shares usb33 (node usb33) on domain ID 2
D/TC:0 0 call_initcalls:40 level 7 stm32_rng_release()
D/TC:0 0 call_initcalls:40 level 7 regulator_core_cleanup()
F/TC:0 0 regulator_core_cleanup:1008
D/TC:0 0 regulator_core_cleanup:1012 disable usb33
D/TC:0 0 regulator_core_cleanup:1012 disable reg18
D/TC:0 0 regulator_core_cleanup:1012 disable reg11
D/TC:0 0 call_initcalls:40 level 7 release_probe_lists()
D/TC:0 0 call_finalcalls:59 level 1 release_external_dt()
I/TC: Primary CPU switching to normal world boot

<debug_uart>
serial_stm32 serial@40010000: pinctrl_select_state_full: uclass_get_device_by_phandle_id: err=-19
serial_stm32 serial@40010000: pinctrl_select_state_full: uclass_get_device_by_phandle_id: err=-19
serial_stm32 serial@40010000: pinctrl_select_state_full: uclass_get_device_by_phandle_id: err=-19
serial_stm32 serial@40010000: pinctrl_select_state_full: uclass_get_device_by_phandle_id: err=-19
No serial driver found
resetting ...
System reset not supported on this platform
### ERROR ### Please RESET the board ###

 

mx-u-boot.dts

 

 

/ {

	/* USER CODE BEGIN root */

	aliases{
		mmc0 = &sdmmc1;
	};

	config{
		u-boot,mmc-env-partition = "u-boot-env";
	};

	/* USER CODE END root */

}; /*root*/

/* USER CODE BEGIN addons */
&uart4{
	u-boot,dm-pre-reloc;
};

&uart4_pins_mx {
	u-boot,dm-pre-reloc;
	pins1 {
		u-boot,dm-pre-reloc;
	};
	pins2 {
		u-boot,dm-pre-reloc;
	};
};

 

 

mx.dts

 

 

aliases{
		serial0 = &uart4;
	};

	chosen{
		stdout-path = "serial0:115200n8";
		#address-cells = <1>;
		#size-cells = <1>;
		ranges;

		framebuffer{
			compatible = "simple-framebuffer";
			clocks = <&rcc LTDC_PX>;
			status = "disabled";
		};
	};

...
&uart4{
	pinctrl-names = "default", "idle", "sleep";
	pinctrl-0 = <&uart4_pins_mx>;
	pinctrl-1 = <&uart4_idle_pins_mx>;
	pinctrl-2 = <&uart4_sleep_pins_mx>;
	status = "okay";

	/* USER CODE BEGIN uart4 */
	/delete-property/ dmas;
	/delete-property/ dma-names;
	/* USER CODE END uart4 */
};

 

 

I can't see anything related in optee.dts what should be enabled to get access to UART4 in u-boot. So what am I missing? Where could I start to look? And what is this error? Is it related to UART4? Well, at least it can print the last error messages to it.

This topic has been closed for replies.

7 replies

PatrickF
ST Employee
July 25, 2024
In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
jhi
jhiAuthor
Senior
July 25, 2024

Yes I already saw it, but the base address (0x40010000) is correct for the UART4 (it is the default). And there are no switches in OP-TEE for UART4 as there are for USART2.

jhi
jhiAuthor
Senior
July 25, 2024

Here are my device tree files.

It is possible to attach only 3 files so the uboot-u-boot.dts is here:

// SPDX-License-Identifier: (GPL-2.0-or-later OR BSD-3-Clause)
/*
 * Copyright (C) 2023, STMicroelectronics - All Rights Reserved
 * Author: STM32CubeMX code generation for STMicroelectronics.
 */

/* For more information on Device Tree configuration, please refer to
 * https://wiki.st.com/stm32mpu/wiki/Category:Device_tree_configuration
 */

/* USER CODE BEGIN includes */
#include "stm32mp13-u-boot.dtsi"
/* USER CODE END includes */

/ {

	/* USER CODE BEGIN root */

	aliases{
		mmc0 = &sdmmc1;
	};

	config{
		u-boot,mmc-env-partition = "u-boot-env";
	};

	/* USER CODE END root */

}; /*root*/

/* USER CODE BEGIN addons */
&uart4{
	u-boot,dm-pre-reloc;
};

&uart4_pins_mx {
	u-boot,dm-pre-reloc;
	pins1 {
		u-boot,dm-pre-reloc;
	};
	pins2 {
		u-boot,dm-pre-reloc;
	};
};
/* USER CODE END addons */

 

jhi
jhiAuthor
Senior
July 29, 2024

I have tried to debug this by adding print statements to serial-uclass.c.

In a function serial_check_stdout the chosen console is found serial0:115200n8, node 7780. Later the device uclass ID is UCLASS_SERIAL, but then the device_probe returns -ENODEV = No such device.

I did dump the tree of all devices

Class Index Probed Driver Name
-----------------------------------------------------------
 root 0 [ + ] root_driver root_driver
 simple_bus 0 [ ] simple_bus |-- soc
 clk 0 [ ] fixed_clock |-- clk-mco1
 serial 0 [ ] serial_stm32 `-- serial@40010000

So the serial is found. 

uclass

uclass 95: serial
0 serial@40010000 @ c02803fc, seq 0

Driver

serial_stm32 095 serial serial@40010000

So any ideas why it still complains that it can't find the device?

jhi
jhiAuthor
Senior
July 29, 2024

I have forgotten to write, that I'm using the bootlin buildroot release st/2023.02.10

jhi
jhiAuthor
Senior
July 30, 2024

I went down the rabbit hole and managed to find, that the problem is clock, but I still don't know what is wrong:

uclass_find_device_by_ofnode (uclass.c) tries to find device node for rcc@50000000. uclass_get will find it with the key 29 

 

Driver uid uclass Devices
----------------------------------------------------------
stm32mp13_clk 029 clk <none>

 

and uclass_foreach_dev(dev, uc) do not anything as us->(I don't know which one) is NULL and then the uclass_find_device_by_ofnode will return -ENODEV.

 

@PatrickF  I would really appreciate a little help from your side. I don't know what the purpose of this community is, when you never get any answer. I still have few questions open and never got answer for those. I can also see, that there are lot of other questions from other users without any reaction from your side.

Visitor II
February 5, 2025

Hi Jhi,

I face similar issues, did you get the answer for it?