STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Connecting cubeMX generated dts file with yocto

Hi everyone,I am using stm32mp157f-dk2 with openSTLinux-5.4-dunfell-eglf distribution.​I would like to configure my device tree using cubeMX.​The generated dts file seems OK to me. However, how can I tell yocto to use my newly generated device tree?​...

WLeun.3 by Associate III
  • 2754 Views
  • 11 replies
  • 0 kudos

Seeed Studio SOM not behaving on shutdown

I have a 3rd party SOM (seeed studio Odyssey). When I edit the .dts file in the tf-a-stm32mp1/fdts directory and add: &pwr_regulators { system_suspend_supported_soc_modes = < STM32_PM_CSLEEP_RUN STM32_PM_CSTOP_...

BBeck.1 by Associate II
  • 1410 Views
  • 1 replies
  • 0 kudos

Interfacing with SN65DSI83 : DSI TO BRIDGE

Hi all,I am trying to interface SN65DSI83 with STM32MP1.Below is my device tree:&ltdc{   status = "okay";   /* USER CODE BEGIN ltdc */   port { #address-cells = <1>; #size-cells = <0>;   ltdc_ep0_out: endpoint@0 { reg = <0>; remot...

NPal.2 by Senior
  • 2770 Views
  • 7 replies
  • 0 kudos

Resolved! eMMC Programming for Mass Production

Hello,What is the best (fastest and reliable) way to program a blank eMMC for mass production? In my custom board, the device will boot from eMMC, no SD card is available. The default pins are shown in the link below. For other data pins is there an...

JDave.4 by Associate III
  • 2760 Views
  • 7 replies
  • 0 kudos

stm32mp157c nand flash u-boot configuration

I am using stm32mp157c and working initialize mtd nand flash w25n512.i was able to run it on kernel mode. Kernel device tree is;aliases { spinand0 = &qspi; }; ...   &qspi { pinctrl-names = "default"; pinctrl-0 = <&quadspi_pins_mx>; num-cs = <0x...

aliMesut by Associate III
  • 1011 Views
  • 2 replies
  • 0 kudos

Whitepaper: Protecting OEM assets and ensuring firmware integrity through STM32 and open-source solutions

Learn how to protect OEM assets and ensure integrity using open-source softwareDownload our whitepaper to better understand these strategies:Secure Boot: How it works and why it is importantHow chain-of-trust mechanisms protect OEM and user dataSecur...

0693W00000KaZJ6QAN.png

STM32MP157C-DK2 board boot at panic mode

I flashed the board with dd command and tried either flashing whole SD card with the .raw image and each partition separately as well, it came up at panic mode. The image is en.FLASH-stm32mp1-openstlinux-5-10-dunfell-mp1-21-11-17_tar_v3.1.0. Does any...

DZ.2 by Associate II
  • 1162 Views
  • 8 replies
  • 0 kudos