ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Write NDEF with CR95HF

Hello,I downloaded STM32CubeExpansion_NFC3_V1.4.0.I use the example projectCR95HF_TagDetect with the board X-NUCLEO-NFC03A1 and the board NUCLEO-F103RB.I use smartphone Sony Xperia L1 (TT4B) an Samsung Galaxy S7 (TT4A).I want test the function NDEF_W...

Resolved! Fast Write on ST25DV error

Hi,I'm trying to use the mailbox of the ST25DV64K on an android application.The Fast Read is ok. But the Fast Write is crashing with an exception.... And the mailbox is correctly written...When I execute the function "mNfcTag.FastWriteMailboxMessage(...

xNiux by Associate II
  • 987 Views
  • 4 replies
  • 0 kudos

Resolved! what configuration to be set to enter the ST25R3911B chip in low power mode & should be wakeup if RFID card is detected & give the interrupt on IRQ pin to wake up the external MCU?

In example code in library STM32CubeExpansion_NFC5_V1.3.0 for STM32L476RG-Nucleo, after pressing user BUTTON, it enters in low power mode. When it should be wake up, after again pressing user BUTTON or After detecting RFID tag? What is the program fl...

RP by Associate II
  • 751 Views
  • 1 replies
  • 0 kudos