2013-08-22 12:03 AM
Hello, I am trying to make my m24lr discovery board work under Linux.
I've seen that ST provides a DLL to communicate with the green board under windows, but I'd like to use it under Linux. As far as I've seen, it is a HID device, but even by reading the source codice for its microcontroller, I've been only able to understand that the firmware forwards the commands to the CR95HF, but I was not able to understand the format of the commands. Do you have a working code to use that board under linux? Or do you have a bit more documentation, so that I can try to use the board with libusb? Thank you Ottavio #cr95hf #linux-driver-cr95hf #linux #linux-driver-cr95hfSolved! Go to Solution.
2015-11-13 5:44 AM
Hello,
The source files are located in theSTSW-95HF004 web site on st.com, here below you will find the link:
http://www.st.com/web/en/catalog/tools/FM147/SC1871/PF262137?s_searchtype=keyword
# I hope this can be helpful, Have a nice day.2013-08-23 12:13 AM
AN3954: Developing your own Visual Basic or C/C++ application on a DEMO-CR95HF-A demonstration board
Have a nice day, All the best , ST NFC/RFID dynamic tag2013-08-29 12:41 AM
My address is ottavio at campana.vi.it
I already studied the document you're mentioning, but my problem is that I'd like to attach the green board to an arm-based linux system, thus I need to understand how I can make the reader work with linux.2013-12-11 4:46 AM
Hello,
I also need to get this M24LR discovery kit working on a linux system. Right now, I use you dll on a windows based PC, but the next step is to move it across to an arm based linux micro-computer. Do you have a linux driver equivalent to the widows dll? My email address, if you need it is charles.whitmore at btinternet.comthanks & regards Charles2015-03-03 1:02 PM
Hello,
I also need information about communication protocol between MB1054A and HID (I am using Linux,I do not have
the ability to use
DLL library) my email: denis.krasutsk(d_o_g)cedoni.com Best Regards, Krasutski Denis.2015-03-04 3:51 PM
Sorry, I made a mistake in my email: denis_krasutski@cedoni.com
2015-06-26 7:05 AM
Hello Denis ,
is this helping you also? Have a nice day, ST NFC/RFID Support2015-08-18 9:03 AM
Hello,
same thing here. The App-Note ''AN4593'' looks great. But where do I find the actual Library files mentioned? Or did I missed something? I would appreciate if you can send me the required files.Mail: Timo.Goestenkors at fh-bielefeld.de
Best regards2015-11-13 5:44 AM
Hello,
The source files are located in theSTSW-95HF004 web site on st.com, here below you will find the link:
http://www.st.com/web/en/catalog/tools/FM147/SC1871/PF262137?s_searchtype=keyword
# I hope this can be helpful, Have a nice day.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.