cancel
Showing results for 
Search instead for 
Did you mean: 

ST95HF Error Codes

oliver239955
Associate II
Posted on October 19, 2015 at 06:41

Hi Guys,

I got problems in the calibration-process (same routine like in the ST95HF Eval Firmware). I should get Responses of the ST95HF like ''0x00 0x01 0x01'' or ''0x00 0x01 0x02'' to get the DAC Data High border. But instead the Repsonses I should get, I get ''0x00 0x01 0x80''. The Datasheet says something like that to the Error Code 0x80:

EFrameRecvOK

Frame correctly received (additionally see

CRC/Parity information)

But that really doesn't help me. I also get sometimes the Error Code 0x82.

Is there an application note, which recommends what o do with the different error codes?

Thanks a lot!

#st95hf-cr95hf-95hf-error-codes
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Nickname5101_O
Associate II
Posted on November 17, 2015 at 14:16

Hello,

do you check forst the communication with ST95HF

What is the sent command ?

have look below to the flow of a correct Tag calibration  seqence

11-17-2015 14:13:49 >>> CR95HFDLL_ECHO

<<< 5500

11-17-2015 14:13:49 >>> -> 1st step : VERIFY detection with DacDataH=0x00 (min value)

11-17-2015 14:13:49 >>> CR95HFDll_STCmd, 01 070E03A100F801180020606000003F01

<<< 000102

11-17-2015 14:13:49 >>> -> 2nd step : VERIFY no detection with DacDataH=0xFC (max value)

11-17-2015 14:13:50 >>> CR95HFDll_STCmd, 01 070E03A100F801180020606000FC3F01

<<< 000101

11-17-2015 14:13:50 >>> -> 3rd step : Calibration with DacDataH=0x7C

11-17-2015 14:13:50 >>> CR95HFDll_STCmd, 01 070E03A100F8011800206060007C3F01

<<< 000101

11-17-2015 14:13:50 >>> -> 4th step : Calibration with DacDataH=0x3C

11-17-2015 14:13:51 >>> CR95HFDll_STCmd, 01 070E03A100F8011800206060003C3F01

<<< 000102

11-17-2015 14:13:51 >>> -> 5th step : Calibration with DacDataH=0x5C

11-17-2015 14:13:52 >>> CR95HFDll_STCmd, 01 070E03A100F8011800206060005C3F01

<<< 000102

11-17-2015 14:13:52 >>> -> 6th step : Calibration with DacDataH=0x6C

11-17-2015 14:13:52 >>> CR95HFDll_STCmd, 01 070E03A100F8011800206060006C3F01

<<< 000101

11-17-2015 14:13:52 >>> -> 7th step : Calibration with DacDataH=0x64

11-17-2015 14:13:53 >>> CR95HFDll_STCmd, 01 070E03A100F801180020606000643F01

<<< 000102

11-17-2015 14:13:53 >>> -> 8th step : Calibration with DacDataH=0x68

11-17-2015 14:13:53 >>> CR95HFDll_STCmd, 01 070E03A100F801180020606000683F01

<<< 000102

11-17-2015 14:13:53 >>> ---> Calibration result : DacDataL = 0x60 / DacDataH = 0x70

View solution in original post

1 REPLY 1
Nickname5101_O
Associate II
Posted on November 17, 2015 at 14:16

Hello,

do you check forst the communication with ST95HF

What is the sent command ?

have look below to the flow of a correct Tag calibration  seqence

11-17-2015 14:13:49 >>> CR95HFDLL_ECHO

<<< 5500

11-17-2015 14:13:49 >>> -> 1st step : VERIFY detection with DacDataH=0x00 (min value)

11-17-2015 14:13:49 >>> CR95HFDll_STCmd, 01 070E03A100F801180020606000003F01

<<< 000102

11-17-2015 14:13:49 >>> -> 2nd step : VERIFY no detection with DacDataH=0xFC (max value)

11-17-2015 14:13:50 >>> CR95HFDll_STCmd, 01 070E03A100F801180020606000FC3F01

<<< 000101

11-17-2015 14:13:50 >>> -> 3rd step : Calibration with DacDataH=0x7C

11-17-2015 14:13:50 >>> CR95HFDll_STCmd, 01 070E03A100F8011800206060007C3F01

<<< 000101

11-17-2015 14:13:50 >>> -> 4th step : Calibration with DacDataH=0x3C

11-17-2015 14:13:51 >>> CR95HFDll_STCmd, 01 070E03A100F8011800206060003C3F01

<<< 000102

11-17-2015 14:13:51 >>> -> 5th step : Calibration with DacDataH=0x5C

11-17-2015 14:13:52 >>> CR95HFDll_STCmd, 01 070E03A100F8011800206060005C3F01

<<< 000102

11-17-2015 14:13:52 >>> -> 6th step : Calibration with DacDataH=0x6C

11-17-2015 14:13:52 >>> CR95HFDll_STCmd, 01 070E03A100F8011800206060006C3F01

<<< 000101

11-17-2015 14:13:52 >>> -> 7th step : Calibration with DacDataH=0x64

11-17-2015 14:13:53 >>> CR95HFDll_STCmd, 01 070E03A100F801180020606000643F01

<<< 000102

11-17-2015 14:13:53 >>> -> 8th step : Calibration with DacDataH=0x68

11-17-2015 14:13:53 >>> CR95HFDll_STCmd, 01 070E03A100F801180020606000683F01

<<< 000102

11-17-2015 14:13:53 >>> ---> Calibration result : DacDataL = 0x60 / DacDataH = 0x70